The INDFn registers are not physical registers. Any instruction that accesses an
INDFn register actually accesses the register at the address specified by the File
Select Registers (FSR). If the FSRn address specifies one of the two INDFn registers,
the read will return ‘0
’ and the write will not occur (though Status
bits may be affected). The FSRn register value is created by the pair FSRnH and
FSRnL.