Interrupt latency is defined as the time from when the interrupt event occurs to the time
code execution at the interrupt vector begins. The interrupt is sampled during Q1 of the
instruction cycle. The actual interrupt latency then depends on the instruction that is
executing at the time the interrupt is detected. See the following figures for more
details.
Figure 1. Interrupt Latency
Figure 2. INT Pin Interrupt
Timing
Notes:
- 1.INTF flag is sampled here (every Q1).
- 2.Asynchronous interrupt
latency = 3-5 TCY. Synchronous latency = 3-4 TCY,
where TCY = instruction cycle time. Latency is the same
whether Inst (PC) is a single cycle or a 2-cycle instruction.
- 3.For minimum width of INT
pulse, refer to AC specifications in the “Electrical Specifications” chapter.
- 4.INTF may be set any time
during the Q4-Q1 cycles.