PMU_ConfigCurrentSensor Function
C
bool PMU_ConfigCurrentSensor(bool enable);Description
This routine will configure the BUCK current sensor. It only can be configured when the power mode is set as PMU_MODE_BUCK_PSM. Disable current sensor can improve the current consumption of sleep mode.
Parameters
bool Enable/Disable BUCK current sensor false: Disable true : Enable
Returns
bool - true is success false is fail due to power mode is not in PMU_MODE_BUCK_PSM