SX_CM_LOAD_MASK
C
typedef int (*FUNC_SX_CM_LOAD_MASK)(struct sxcmmask *c, uint32_t value); #define SX_CM_LOAD_MASK ((FUNC_SX_CM_LOAD_MASK)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_SX_CM_LOAD_MASK)))
Description
Loads random used in the AES counter-measures.
Counter-measures are available for the AES, if enabled in HW. This function initializes the user allocated object \p c with a new counter-measures mask load operation context and reserves the HW resource. After the initialization of \p c, this function starts the load of the counter-measure cryptographically secure random \p value. The function will return immediately. No data will be received for the load operation. The operation is considered successful if the status returned by SX_CM_LOAD_MASK_WAIT() or SX_CM_LOAD_MASK_STATUS() is ::SX_OK. remark - it is under the user responsibility to call it after system boot (not automatically called).
Parameters
| Param | Description |
|---|---|
| c | counter-measures mask load operation context |
| value | counter-measures random value to be loaded |
Returns
SX_OK SX_ERR_INCOMPATIBLE_HW SX_ERR_RETRY
SX_CM_LOAD_MASK_WAIT
C
typedef int (*FUNC_SX_CM_LOAD_MASK_WAIT)(struct sxcmmask *c); #define SX_CM_LOAD_MASK_WAIT ((FUNC_SX_CM_LOAD_MASK_WAIT)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_SX_CM_LOAD_MASK_WAIT)))
Description
Waits until the given AES counter-measures load operation has finished. This function returns when the counter-measures load operation was successfully completed, or when an error has occurred that caused the operation to terminate. The return value of this function is the operation status. After this call, all resources have been released and \p c cannot be used again unless SX_CM_LOAD_MASK() is used. pre - SX_CM_LOAD_MASK() function must be called first remark - this function is blocking until operation finishes.
Parameters
| Param | Description |
|---|---|
| c | counter-measures mask load operation context |
See
SX_CM_LOAD_MASK_STATUS()
Returns
SX_OK SX_ERR_INCOMPATIBLE_HW SX_ERR_RETRY
SX_CM_LOAD_MASK_STATUS
C
typedef int (*FUNC_SX_CM_LOAD_MASK_STATUS)(struct sxcmmask *c); #define SX_CM_LOAD_MASK_STATUS ((FUNC_SX_CM_LOAD_MASK_STATUS)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_SX_CM_LOAD_MASK_STATUS)))
Description
Returns the status of the given AES counter-measures load operation context.
If the operation is still ongoing, return ::SX_ERR_HW_PROCESSING. In that case, the user can retry later.
When this function returns with a code different than ::SX_ERR_HW_PROCESSING, the counter-measures mask load operation has ended and all resources used by counter-measures mask load operation context \p c have been released. In this case, \p c cannot be used for a new operation until SX_CM_LOAD_MASK() is called again. pre - SX_CM_LOAD_MASK() function must be called first
Parameters
| Param | Description |
|---|---|
| c | counter-measures mask load operation context |
See
SX_CM_LOAD_MASK_STATUS()
Returns
SX_OK SX_ERR_UNITIALIZED_OBJ SX_ERR_HW_PROCESSING SX_ERR_DMA_FAILED