CRM_OK Macro
C
#define CRM_OK 0
Description
The function or operation succeeded
CRM_ERR_INVALID_PARAM Macro
C
#define CRM_ERR_INVALID_PARAM 1
Description
The function or parameter was given an invalid parameter
CRM_ERR_UNKNOWN_ERROR Macro
C
#define CRM_ERR_UNKNOWN_ERROR 2
Description
Unknown error
CRM_ERR_BUSY Macro
C
#define CRM_ERR_BUSY 3
Description
The operation is still executing
CRM_ERR_NOT_QUADRATIC_RESIDUE Macro
C
#define CRM_ERR_NOT_QUADRATIC_RESIDUE 4
Description
The input operand is not a quadratic residue
CRM_ERR_COMPOSITE_VALUE Macro
C
#define CRM_ERR_COMPOSITE_VALUE 5
Description
The input value for Rabin-Miller test is a composite value
CRM_ERR_NOT_INVERTIBLE Macro
C
#define CRM_ERR_NOT_INVERTIBLE 6
Description
Inversion of a non-invertible value
CRM_ERR_INVALID_SIGNATURE Macro
C
#define CRM_ERR_INVALID_SIGNATURE 7
Description
The signature is not valid
CRM_ERR_NOT_IMPLEMENTED Macro
C
#define CRM_ERR_NOT_IMPLEMENTED 8
Description
Functionality not supported
CRM_ERR_POINT_AT_INFINITY Macro
C
#define CRM_ERR_POINT_AT_INFINITY 9
Description
The operand is point at infinity
CRM_ERR_INVALID_MODULUS Macro
C
#define CRM_ERR_INVALID_MODULUS 11
Description
The modulus has unexpected value
CRM_ERR_POINT_NOT_ON_CURVE Macro
C
#define CRM_ERR_POINT_NOT_ON_CURVE 12
Description
The input point is not on the defined elliptic curve
CRM_ERR_OUT_OF_RANGE Macro
C
#define CRM_ERR_OUT_OF_RANGE 10
Description
The input value is outside the expected range
CRM_ERR_OPERAND_TOO_LARGE Macro
C
#define CRM_ERR_OPERAND_TOO_LARGE 13
Description
The input operand is too large
CRM_ERR_PLATFORM_ERROR Macro
C
#define CRM_ERR_PLATFORM_ERROR 14
Description
A platform specific error
CRM_ERR_EXPIRED Macro
C
#define CRM_ERR_EXPIRED 15
Description
The evaluation period for the product expired
CRM_ERR_IK_MODE Macro
C
#define CRM_ERR_IK_MODE 16
Description
The hardware is still in IK mode
CRM_ERR_INVALID_CURVE_PARAM Macro
C
#define CRM_ERR_INVALID_CURVE_PARAM 17
Description
The parameters of the elliptic curve are not valid
CRM_DESCRIBE_STATUSCODE
C
typedef const char *(*FUNC_CRM_DESCRIBE_STATUSCODE)(int code); #define CRM_DESCRIBE_STATUSCODE ((FUNC_CRM_DESCRIBE_STATUSCODE)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_DESCRIBE_STATUSCODE)))
Description
Return a brief text string describing the given status code.
Parameters
| Param | Description |
|---|---|
| code | Value of status code |
Returns
Text string describing status code