GUID 5694B173 D2C7 413A B5FB C2B0F23E116C
C
CRM_MAC_CREATE_HMAC_SHA2_256
C
typedef int (*FUNC_CRM_MAC_CREATE_HMAC_SHA256)(struct crmmac *c, struct crmkeyref *keyref); #define CRM_MAC_CREATE_HMAC_SHA2_256 ((FUNC_CRM_MAC_CREATE_HMAC_SHA256)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_MAC_CREATE_HMAC_SHA2_256)))
Description
Prepares a HMAC SHA256 MAC operation
This function initializes the user allocated object \p c with a new MAC operation context and reserves the HW resource. After successful execution of this function, the context \p c can be passed to any of the hashing functions (except the ones that are specific to context-saving).
Parameters
| Param | Description |
|---|---|
| c | MAC Operation context |
| hmackey | HMAC key |
| ksz | Size in bytes of the HMAC key, can be any size |
Returns
CRM_OK CRM_ERR_INCOMPATIBLE_HW CRM_ERR_RETRY
CRM_MAC_CREATE_HMAC_SHA2_384
C
typedef int (*FUNC_CRM_MAC_CREATE_HMAC_SHA384)(struct crmmac *c, struct crmkeyref *keyref); #define CRM_MAC_CREATE_HMAC_SHA2_384 ((FUNC_CRM_MAC_CREATE_HMAC_SHA384)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_MAC_CREATE_HMAC_SHA2_384)))
Description
Prepares a HMAC SHA384 MAC operation This function initializes the user allocated object \p c with a new MAC operation context and reserves the HW resource. After successful execution of this function, the context \p c can be passed to any of the hashing functions (except the ones that are specific to context-saving). remark - \p hmackey buffer should not be changed until the operation is completed.
Parameters
| Param | Description |
|---|---|
| c | MAC Operation context |
| hmackey | HMAC key |
| ksz | Size in bytes of the HMAC key, can be any size |
Returns
CRM_OK CRM_ERR_INCOMPATIBLE_HW CRM_ERR_RETRY
CRM_MAC_CREATE_HMAC_SHA2_512
C
typedef int (*FUNC_CRM_MAC_CREATE_HMAC_SHA2_512)(struct crmmac *c, struct crmkeyref *keyref); #define CRM_MAC_CREATE_HMAC_SHA2_512 ((FUNC_CRM_MAC_CREATE_HMAC_SHA2_512)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_MAC_CREATE_HMAC_SHA2_512)))
Description
Prepares a HMAC SHA512 MAC operation This function initializes the user allocated object \p c with a new MAC operation context and reserves the HW resource. After successful execution of this function, the context \p c can be passed to any of the hashing functions (except the ones that are specific to context-saving). remark - \p hmackey buffer should not be changed until the operation is completed.
Parameters
| Param | Description |
|---|---|
| c | MAC Operation context |
| hmackey | HMAC key |
| ksz | Size in bytes of the HMAC key, can be any size |
Returns
CRM_OK CRM_ERR_INCOMPATIBLE_HW CRM_ERR_RETRY
CRM_MAC_CREATE_HMAC_SHA1
C
typedef int (*FUNC_CRM_MAC_CREATE_HMAC_SHA1)(struct crmmac *c, struct crmkeyref *keyref); #define CRM_MAC_CREATE_HMAC_SHA1 ((FUNC_CRM_MAC_CREATE_HMAC_SHA1)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_MAC_CREATE_HMAC_SHA1)))
Description
Prepares a HMAC SHA1 MAC operation This function initializes the user allocated object \p c with a new MAC operation context and reserves the HW resource. After successful execution of this function, the context \p c can be passed to any of the hashing functions (except the ones that are specific to context-saving). remark - \p hmackey buffer should not be changed until the operation is completed.
Parameters
| Param | Description |
|---|---|
| c | MAC Operation context |
| hmackey | HMAC key |
| ksz | Size in bytes of the HMAC key, can be any size |
Returns
CRM_OK CRM_ERR_INCOMPATIBLE_HW CRM_ERR_RETRY
CRM_MAC_CREATE_HMAC_SHA2_224
C
typedef int (*FUNC_CRM_MAC_CREATE_HMAC_SHA224)(struct crmmac *c, struct crmkeyref *keyref); #define CRM_MAC_CREATE_HMAC_SHA2_224 ((FUNC_CRM_MAC_CREATE_HMAC_SHA224)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_MAC_CREATE_HMAC_SHA2_224)))
Description
Prepares a HMAC SHA224 MAC operation This function initializes the user allocated object \p c with a new MAC operation context and reserves the HW resource. After successful execution of this function, the context \p c can be passed to any of the hashing functions (except the ones that are specific to context-saving). remark - \p hmackey buffer should not be changed until the operation is completed.
Parameters
| Param | Description |
|---|---|
| c | MAC Operation context |
| hmackey | HMAC key |
| ksz | Size in bytes of the HMAC key, can be any size |
Returns
CRM_OK CRM_ERR_INCOMPATIBLE_HW CRM_ERR_RETRY