crm_pk_point Struct
C
struct crm_pk_point {
crm_op *x; /**< x-coordinate */
crm_op *y; /**< y-coordinate */
};Description
Affine point parameter group. This structure is used for point values which are stored in two consecutive locations (x and y0
crm_ecjpake_generate_zkp_go
C
struct crm_pk_dreq crm_ecjpake_generate_zkp_go(
const struct crm_pk_ecurve *curve,
const crm_op *v,
const crm_op *x,
const crm_op *h)Description
Asynchronous EC J-PAKE proof generation
Start a EC J-PAKE proof generation operation on the accelerator and return immediately.
When the operation finishes on the accelerator, call crm_async_generate_zkp_end()
Parameters
| Param | Description |
|---|---|
| curve | Elliptic curve on which to perform the operation |
| v | Random input ( < n ) |
| x | Exponent |
| h | Hash digest |
Truncation or padding should be done by user application
Returns
Acquired acceleration request for this operation
crm_ecjpake_generate_zkp_end
C
void crm_ecjpake_generate_zkp_end(
crm_pk_accel *req,
crm_op *r)
Description
Finish asynchronous (non-blocking) EC J-PAKE proof generation.
Get the output operands of the EC J-PAKE proof generation and release the reserved resources.
The operation on the accelerator must be finished before calling this function.
Parameters
| Param | Description |
|---|---|
| req | The previously acquired acceleration request for this operation |
| r | The resulting value |
Returns
None
crm_ecjpake_generate_zkp
C
int crm_ecjpake_generate_zkp(
const struct crm_pk_ecurve *curve,
const crm_op *v,
const crm_op *x,
const crm_op *h,
crm_op *r
)Description
Perform an EC J-PAKE proof generation
The proof generation has the following steps:
- r = (v - (x * h)) % n
Parameters
| Param | Description |
|---|---|
| curve | Elliptic curve on which to perform the operation |
| v | Random input ( < n ) |
| x | Exponent |
| h | Hash digest |
Truncation or padding should be done by user application
See
crm_async_ecjpake_generate_zkp_go(), crm_async_ecjpake_generate_zkp_end() for an asynchronous version
Returns
CRM_OK CRM_ERR_OUT_OF_RANGE CRM_ERR_POINT_NOT_ON_CURVE CRM_ERR_NOT_INVERTIBLE CRM_ERR_UNKNOWN_ERROR CRM_ERR_BUSY CRM_ERR_NOT_IMPLEMENTED CRM_ERR_OPERAND_TOO_LARGE CRM_ERR_PLATFORM_ERROR CRM_ERR_EXPIRED
crm_ecjpake_verify_zkp_go
C
struct crm_pk_dreq crm_ecjpake_verify_zkp_go(
const struct crm_pk_ecurve *curve,
const struct crm_pk_point *v,
const struct crm_pk_point *x,
const crm_op *r,
const crm_op *h,
const struct crm_pk_point *g)Description
Asynchronous EC J-PAKE proof verification
Start an EC J-PAKE proof verification operation on the accelerator and return immediately. When the operation finishes on the accelerator, call crm_ecjpake_verify_zkp_end()
Parameters
| Param | Description |
|---|---|
| curve | Elliptic curve on which to perform the operation |
| v | POint on the curve |
| x | Point on the curve |
| r | Proof to be verified |
| h | Hash digest |
| g | Point on the curve (Optional, pass CRM_PT_CURVE_GENERATOR to use the curve generator point) |
Truncation or padding should be done by user application
See
crm_async_ecjpake_generate_zkp_go(), crm_async_ecjpake_generate_zkp_end() for an asynchronous version
Returns
Acquired acceleration request for this operation
crm_ecjpake_verify_zkp_end
C
void crm_ecjpake_verify_zkp_end(
crm_pk_accel *req
)
Description
Finish asynchronous (non-blocking) EC J-PAKE proof verification
Finishes the EC J-PAKE proof verification and releases the reserved resources. The operation on the accelerator must be finished before calling this function.
Parameters
| Param | Description |
|---|---|
| req | The previously acquired acceleration request for this operation |
Returns
None
crm_ecjpake_verify_zkp
C
int crm_ecjpake_verify_zkp(
const struct crm_pk_ecurve *curve,
const struct crm_pk_point *v,
const struct crm_pk_point *x,
const crm_op *r,
const crm_op *h,
const struct crm_pk_point *g
)Description
Synchronous EC J-PAKE proof verification Start an EC J-PAKE proof verification operation on the accelerator and return immediately. The proof verification has the following steps:
- ( (G * r) + (X * h) ) ?= V
In case of a comparison failure CRM_ERR_INVALID_SIGNATURE shall be returned. When the operation finishes on the accelerator, call crm_ecjpake_verify_zkp_end()
Parameters
| Param | Description |
|---|---|
| curve | Elliptic curve on which to perform the operation |
| v | POint on the curve |
| x | Point on the curve |
| r | Proof to be verified |
| h | Hash digest |
| g | Point on the curve (Optional, pass CRM_PT_CURVE_GENERATOR to use the curve generator point) |
Truncation or padding should be done by user application
See
crm_async_ecjpake_verify_zkp_go(), crm_async_ecjpake_verify_zkp_end() for an asynchronous version
Returns
CRM_OK CRM_ERR_INVALID_SIGNATURE CRM_ERR_OUT_OF_RANGE CRM_ERR_POINT_NOT_ON_CURVE CRM_ERR_NOT_INVERTIBLE CRM_ERR_UNKNOWN_ERROR CRM_ERR_BUSY CRM_ERR_NOT_IMPLEMENTED CRM_ERR_OPERAND_TOO_LARGE CRM_ERR_PLATFORM_ERROR CRM_ERR_EXPIRED
crm_ecjpake_3pt_add_go
C
struct crm_pk_dreq crm_ecjpake_3pt_add_go(
const struct crm_pk_ecurve *curve,
const struct crm_pk_point *a,
const struct crm_pk_point *b,
const struct crm_pk_point *c)Description
Start a EC J-PAKE 3 point addition operation on the accelerator and return immediately. When the operation finishes on the accelerator, call crm_ecjpake_3pt_add_end()
Parameters
| Param | Description |
|---|---|
| curve | Elliptic curve on which to perform the operation |
| a | Point on the curve |
| b | Point on the curve |
| c | Point on the curve |
Returns
Acquired acceleration request for this operation
crm_ecjpake_3pt_add_end
C
void crm_ecjpake_3pt_add_end(
crm_pk_accel *req,
struct crm_pk_point *gb
)Description
Finish asynchronous (non-blocking) EC J-PAKE 3 point addition. Finishes the EC J-PAKE 3 point addition and releases the reserved resources. The operation on the accelerator must be finished before calling this function.
Parameters
| Param | Description |
|---|---|
| req | The previously acquired acceleration request for this operation |
| gb | The addition result |
Returns
None
crm_ecjpake_3pt_add_go
C
int crm_ecjpake_3pt_add(
const struct crm_pk_ecurve *curve,
const struct crm_pk_point *a,
const struct crm_pk_point *b,
const struct crm_pk_point *c,
struct crm_pk_point *gb
)Description
Synchronous EC J-PAKE 3 point addition Start a EC J-PAKE 3 point addition operation on the accelerator and return immediately. The 3 point addition operation has the following steps:
- gb = a + b + c When the operation finishes on the accelerator, call crm_ecjpake_3pt_add_end()
Parameters
| Param | Description |
|---|---|
| curve | Elliptic curve on which to perform the operation |
| a | Point on the curve |
| b | Point on the curve |
| c | Point on the curve |
| gb | The addition result |
Truncation or padding should be done by user application
See
crm_async_ecjpake_verify_zkp_go(), crm_async_ecjpake_verify_zkp_end() for an asynchronous version
Returns
CRM_OK CRM_ERR_INVALID_SIGNATURE CRM_ERR_OUT_OF_RANGE CRM_ERR_POINT_NOT_ON_CURVE CRM_ERR_NOT_INVERTIBLE CRM_ERR_UNKNOWN_ERROR CRM_ERR_BUSY CRM_ERR_NOT_IMPLEMENTED CRM_ERR_OPERAND_TOO_LARGE CRM_ERR_PLATFORM_ERROR CRM_ERR_EXPIRED
crm_ecjpake_gen_sess_key_go
C
struct crm_pk_dreq crm_ecjpake_gen_sess_key_go(
const struct crm_pk_ecurve *curve,
const struct crm_pk_point *x4,
const struct crm_pk_point *b,
const crm_op *x2,
const crm_op *x2s)Description
Asynchronous EC J-PAKE session key generation tart a EC J-PAKE session key generation operation on the accelerator and return immediately. When the operation finishes on the accelerator, call crm_ecjpake_gen_sess_key_end()
Parameters
| Param | Description |
|---|---|
| curve | The previously acquired acceleration request for this operation |
| x4 | Point on the curve |
| b | Point on the curve |
| x2 | Generated random number |
| x2s | (x2*s) % n |
Truncation or padding should be done by user application
Returns
Acquired acceleration request for this operation
crm_ecjpake_gen_sess_key_end
C
void crm_ecjpake_gen_sess_key_end(
crm_pk_accel *req,
struct crm_pk_point *t)Description
Finish asynchronous (non-blocking) EC J-PAKE session key generation Finishes the EC J-PAKE session key generation operation and releases the reserved resources. The operation on the accelerator must be finished before calling this function.
Parameters
| Param | Description |
|---|---|
| req | The previously acquired acceleration request for this operation |
| t | The result |
Returns
None
crm_ecjpake_3pt_add_go
C
int crm_ecjpake_gen_sess_key(
const struct crm_pk_ecurve *curve,
const struct crm_pk_point *x4,
const struct crm_pk_point *b,
const crm_op *x2,
const crm_op *x2s,
struct crm_pk_point *t
)Description
Synchronous EC J-PAKE session key generation Start a EC J-PAKE session key generation operation on the accelerator and return immediately. The session key generation has the following steps:
- T = (b - (x4 * x2s)) * x2 When the operation finishes on the accelerator, call crm_ecjpake_gen_sess_key_end()
Parameters
| Param | Description |
|---|---|
| curve | Elliptic curve on which to perform the operation |
| x4 | Point on the curve |
| b | Point on the curve |
| x2 | Generated Random number |
| x2s | x2 * password |
Truncation or padding should be done by user application
See
crm_async_ecjpake_gen_sess_key_go(), crm_async_ecjpake_gen_sess_key_end() for an asynchronous version
Returns
CRM_OK CRM_ERR_INVALID_SIGNATURE CRM_ERR_OUT_OF_RANGE CRM_ERR_POINT_NOT_ON_CURVE CRM_ERR_NOT_INVERTIBLE CRM_ERR_UNKNOWN_ERROR CRM_ERR_BUSY CRM_ERR_NOT_IMPLEMENTED CRM_ERR_OPERAND_TOO_LARGE CRM_ERR_PLATFORM_ERROR CRM_ERR_EXPIRED
crm_ecjpake_gen_step_2_go
C
struct crm_pk_dreq crm_ecjpake_gen_step_2_go(
const struct crm_pk_ecurve *curve,
const struct crm_pk_point *x4,
const struct crm_pk_point *x3,
const struct crm_pk_point *x1,
const crm_op *x2s,
const crm_op *s)Description
Asynchronous EC J-PAKE step 2 calculation Start an EC J-PAKE step 2 calculation operation on the accelerator and return immediately. When the operation finishes on the accelerator, call crm_ecjpake_gen_step_2_end()
Parameters
| Param | Description |
|---|---|
| curve | The previously acquired acceleration request for this operation |
| x4 | Point on the curve |
| x3 | Point on the curve |
| x1 | Point on the curve |
| x2s | (x2*s) % n |
| s | password |
Truncation or padding should be done by user application
Returns
Acquired acceleration request for this operation
crm_ecjpake_gen_step_2_end
C
void crm_ecjpake_gen_step_2_end(
crm_pk_accel *req,
struct crm_pk_point *a,
crm_op *x2s,
struct crm_pk_point *ga)Description
Finish an asynchronous (non-blocking) EC J-PAKE step 2 calculation Finishes the EC J-PAKE step 2 calculation operation and releases the reserved resources. The operation on the accelerator must be finished before calling this function.
Parameters
| Param | Description |
|---|---|
| req | The previously acquired acceleration request for this operation |
| a | Point on the curve |
| x2s | Generated random * password |
| ga | Point on the curve |
Returns
None
crm_ecjpake_gen_step_2
C
int crm_ecjpake_gen_step_2(
const struct crm_pk_ecurve *curve,
const struct crm_pk_point *x4,
const struct crm_pk_point *x3,
const struct crm_pk_point *x1,
const crm_op *x2s,
const crm_op *s,
struct crm_pk_point *a,
crm_op *rx2s,
struct crm_pk_point *ga
)Description
Synchronous EC J-PAKE step 2 calculation Start an EC J-PAKE step 2 calculation operation on the accelerator and return immediately. The step 2 calculation has the following steps:
- ga = x1 + x3 + x4
- rx2s = (x2s * s) % curve.n
- a = ga * rx2s
Parameters
| Param | Description | |:----- |:----------- | PO | curve | Elliptic curve on which to perform the operation | | x4 | Point on the curve | | x3 | Point on the curve | | x1 | Point on the curve | | x2s | Generated random * password | | s | Password | | a | Point on the curve | | rx2s | Generated random * password | | ga | Point on the curve |
Truncation or padding should be done by user application
See
crm_async_ecjpake_gen_step_2_go(), crm_async_ecjpake_gen_step_2_end() for an asynchronous version
Returns
CRM_OK CRM_ERR_INVALID_SIGNATURE CRM_ERR_OUT_OF_RANGE CRM_ERR_POINT_NOT_ON_CURVE CRM_ERR_NOT_INVERTIBLE CRM_ERR_UNKNOWN_ERROR CRM_ERR_BUSY CRM_ERR_NOT_IMPLEMENTED CRM_ERR_OPERAND_TOO_LARGE CRM_ERR_PLATFORM_ERROR CRM_ERR_EXPIRED