crm_pk_constraints Struct
C
struct crm_pk_constraints {
/** Maximum simultaneous requests any application can configure. */
int maxpending;
};Description
CryptoPK and hardware constraints
crm_pk_capabilities Struct
C
struct crm_pk_capabilities {
/** Maximum pending requests at any time. */
int maxpending;
/** Maximum operand size for prime field operands. 0 when not supported. */
int max_gfp_opsz;
/** Maximum operand size for elliptic curve operands. 0 when not supported. */
int max_ecc_opsz;
/** Maximum operand size for binary field operands. 0 when not supported. */
int max_gfb_opsz;
/** Operand size for IK operands. 0 when not supported. */
int ik_opsz;
};Description
Description of the (hardware) accelerator capabilities and features
crm_pk_config Struct
C
struct crm_pk_config {
/** Maximum simultaneous requests the application will start.
*
* Set to 0 to use library default.
*/
int maxpending;
/** Device index to use.
*
* For special use cases with multiple independent hardware
* accelerators. In case of doubt, leave to 0.
*/
int devidx;
/** User memory */
long long *usrmem;
/** Size of user provided memory */
size_t usrmemsz;
/** Personalization string for IK */
uint32_t *personalization;
/** Personalization string size in 32 bit words
*
* If the size is 0 the personalization string
* is considered NULL and will not be used.
*/
int personalization_sz;
};Description
Library configuration for CRM_PK_OPEN()
crm_pk_dreq Struct
C
struct crm_pk_dreq
{
/** The acquired acceleration request **/
crm_pk_accel *req;
/** The status of CRM_PK_ACQUIRE_REQ() **/
int status;
};Description
Encapsulated acceleration request
PK_OP_FLAGS_EDDSA_AX_LSB Macro
C
#define PK_OP_FLAGS_EDDSA_AX_LSB (1 << 29)
Description
Least significant bit of Ax is 1 (flag A)
PK_OP_FLAGS_EDDSA_RX_LSB Macro
C
#define PK_OP_FLAGS_EDDSA_RX_LSB (1 << 30)
Description
Least significant bit of Rx is 1 (flag B)
crm_pk_slot Struct
C
struct crm_pk_slot
{
/** Memory address of the operand slot **/
char *addr;
};Description
Operand slot structure
crm_pk_dblslot Struct
C
struct crm_pk_dblslot
{
/** First slot **/
struct crm_pk_slot a;
/** Second slot **/
struct crm_pk_slot b;
};Description
Pair of slots. Used to store large values
crm_pk_ecurve Struct
C
struct crm_pk_ecurve {
uint32_t curveflags;
int sz;
const char *params;
int offset;
struct crm_pk_cnx *cnx;
};Description
Elliptic curve configuration and parameters.To be used only via the functions in ec_curves.h The internal members of the structure should not be accessed directly
CRM_PK_LIST_CONSTRAINTS
C
typedef struct crm_pk_constraints (*FUNC_CRM_PK_LIST_CONSTRAINTS)(int index, int usermemsz); #define CRM_PK_LIST_CONSTRAINTS ((FUNC_CRM_PK_LIST_CONSTRAINTS)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_LIST_CONSTRAINTS)))
Description
Return CryptoPK constraints If maxpending in crm_pk_constraints is 0, than CryptoPK cannot be used with the given environment.
Parameters
| Param | Description |
|---|---|
| index | index should always be 0 |
| usermemsz | User memory size provided in bytes. Should be non zero with no static memory |
Returns
Constraints of CryptoPK
CRM_PK_FETCH_CAPABILITIES
C
typedef const struct crm_pk_capabilities *(*FUNC_CRM_PK_FETCH_CAPABILITIES)(struct crm_pk_cnx *cnx); #define CRM_PK_FETCH_CAPABILITIES ((FUNC_CRM_PK_FETCH_CAPABILITIES)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_FETCH_CAPABILITIES)))
Description
Return the crypto acceleration capabilities and features
Parameters
| Param | Description |
|---|---|
| cnx | Connection structure obtained through CRM_PK_OPEN() at startup |
Returns
Returns Capabilities of the accelator on success
CRM_PK_OPEN
C
typedef struct crm_pk_cnx *(*FUNC_CRM_PK_OPEN)(struct crm_pk_config *cfg); #define CRM_PK_OPEN ((FUNC_CRM_PK_OPEN)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_OPEN)))
Description
Open CryptoPK and related hardware and allocate internal resources
Parameters
| Param | Description |
|---|---|
| cfg | Configuration to customize CryptoPK to application specific needs |
Returns
NULL on failure Connection structure for future CryptoPK calls on success. Can be used with CryptoPK functions to run operations.
##SEE
CRM_PK_CLOSE()
CRM_PK_CLOSE
C
typedef void (*FUNC_CRM_PK_CLOSE)(struct crm_pk_cnx *cnx); #define CRM_PK_CLOSE ((FUNC_CRM_PK_CLOSE)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_CLOSE)))
Description
Finish using any public key acceleration. No other hardware acceleration function can be called after this.
Parameters
| Param | Description |
|---|---|
| cnx | Connection structure obtained through CRM_PK_OPEN() at startup |
Returns
None
CRM_PK_ACQUIRE_REQ
C
typedef struct crm_pk_dreq (*FUNC_CRM_PK_ACQUIRE_REQ)(struct crm_pk_cnx *cnx, const struct crm_pk_cmd_def *cmd); #define CRM_PK_ACQUIRE_REQ ((FUNC_CRM_PK_ACQUIRE_REQ)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_ACQUIRE_REQ)))
Description
Get a CryptoPK request instance locked to perform the given operation. The returned crm_pk_dreq structure contains a status and a pointer to a reserved hardware accelerator instance. That pointer is only valid and usable if status is non-zero.
Parameters
| Param | Description |
|---|---|
| cnx | Connection structure obtained through CRM_PK_OPEN() at startup |
| cmd | The command definition (for example ::CRM_PK_CMD_MOD_EXP) |
Returns
None
##SEE CRM_PK_RELEASE_REQ()
CRM_PK_GET_REQ_ID
C
typedef unsigned int (*FUNC_CRM_PK_GET_REQ_ID)(crm_pk_accel *req); #define CRM_PK_GET_REQ_ID ((FUNC_CRM_PK_GET_REQ_ID)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_GET_REQ_ID
Description
Return the instance number of the hardware accelerator for this request
Parameters
| Param | Description |
|---|---|
| req | The acceleration request obtained through CRM_PK_ACQUIRE_REQ() |
| cmd | The command definition (for example ::CRM_PK_CMD_MOD_EXP) |
Returns
Instance number of the hardware accelerator for this request
CRM_PK_SET_USER_CONTEXT
C
typedef void (*FUNC_CRM_PK_SET_USER_CONTEXT)(crm_pk_accel *req, void *context); #define CRM_PK_SET_USER_CONTEXT ((FUNC_CRM_PK_SET_USER_CONTEXT)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_SET_USER_CONTEXT)))
Description
Add the context pointer to an acceleration request. The attached pointer can be retrieved by CRM_PK_GET_USER_CONTEXT(). After CRM_PK_RELEASE_REQ(), the context pointer is not available anymore. The context can represent any content the user may associate with the PK request.
Parameters
| Param | Description |
|---|---|
| req | The acquired acceleration request |
Returns
Context pointer from an acceleration request
SEE
CRM_PK_GET_USER_CONTEXT()
CRM_PK_GET_USER_CONTEXT
C
typedef void *(*FUNC_CRM_PK_GET_USER_CONTEXT)(crm_pk_accel *req); #define CRM_PK_GET_USER_CONTEXT ((FUNC_CRM_PK_GET_USER_CONTEXT)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_GET_USER_CONTEXT)))
Description
Get the context pointer from an acceleration request
Parameters
| Param | Description |
|---|---|
| req | The acquired acceleration request |
Returns
None
SEE
CRM_PK_SET_USER_CONTEXT()
CRM_PK_GET_OPSIZE
C
typedef int (*FUNC_CRM_PK_GET_OPSIZE)(crm_pk_accel *req); #define CRM_PK_GET_OPSIZE ((FUNC_CRM_PK_GET_OPSIZE)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_GET_OPSIZE)))
Description
Return the global operands size detected for the request
Parameters
| Param | Description |
|---|---|
| req | The acquired acceleration request |
Returns
Operand size for the request
CRM_PK_LIST_ECC_INSLOTS
C
typedef int (*FUNC_CRM_PK_LIST_ECC_INSLOTS)(crm_pk_accel *req, const struct crm_pk_ecurve *curve, int flags, struct crm_pk_slot *inputs); #define CRM_PK_LIST_ECC_INSLOTS ((FUNC_CRM_PK_LIST_ECC_INSLOTS)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_LIST_ECC_INSLOTS)))
Description
List slots for input operands for an ECC operation. Once the function completes with ::CRM_OK, write each operand to the address found in the corresponding slot. That applies to all ECC operations.
Parameters
| Param | Description |
|---|---|
| req | The acquired acceleration request through CRM_PK_ACQUIRE_REQ() |
| curve | The curve used for that ECC operation |
| flags | Operation specific flags |
| inputs | List of input slots that will be filled in |
Returns
CRM_OK CRM_ERR_OPERAND_TOO_LARGE CRM_ERR_BUSY
CRM_PK_LIST_GFP_INSLOTS
C
typedef int (*FUNC_CRM_PK_LIST_GFP_INSLOTS)(crm_pk_accel *req, const int *opsizes, struct crm_pk_slot *inputs); #define CRM_PK_LIST_GFP_INSLOTS ((FUNC_CRM_PK_LIST_GFP_INSLOTS)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_LIST_GFP_INSLOTS)))
Description
List slots for input operands for an GF(p) modular operation. Once the function completes with ::CRM_OK, write each operands to the address found in the corresponding slot. That applies to all operation except ECC.
Parameters
| Param | Description |
|---|---|
| req | The acquired acceleration request through CRM_PK_ACQUIRE_REQ() |
| opsizes | List of operand sizes |
| inputs | List of input slots that will be filled in |
Returns
CRM_OK CRM_ERR_OPERAND_TOO_LARGE CRM_ERR_BUSY
CRM_PK_RUN
C
typedef void (*FUNC_CRM_PK_RUN)(crm_pk_accel *req); #define CRM_PK_RUN ((FUNC_CRM_PK_RUN)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_RUN)))
Description
Run the operation request in hardware
PRE
To be called after all operands have been written in the slots obtainded with CRM_PK_LIST_ECC_INSLOTS() or CRM_PK_LIST_GFP_INSLOTS(). After that the acceleration request is pending.
POST
The caller should wait until the operation finishes with CRM_PK_WAIT() or do polling by using crm_pk_has_finished().
Parameters
| Param | Description |
|---|---|
| req | The acquired acceleration request through CRM_PK_ACQUIRE_REQ() |
Returns
None
CRM_PK_WAIT
C
typedef int (*FUNC_CRM_PK_WAIT)(crm_pk_accel *req); #define CRM_PK_WAIT ((FUNC_CRM_PK_WAIT)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_WAIT)))
Description
Wait until the current operation finishes. After the operation finishes, return the operation status code.
Parameters
| Param | Description |
|---|---|
| req | The acquired acceleration request through CRM_PK_ACQUIRE_REQ() |
Returns
Any \ref CRM_PK_STATUS "status code"
CRM_PK_CLEARIRQ
C
typedef void (*FUNC_CRM_PK_CLEAR_IRQ)(void); #define CRM_PK_CLEARIRQ ((FUNC_CRM_PK_CLEAR_IRQ)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_CLEARIRQ)))
Description
Clear the interrupt request signal
Parameters
None
Returns
None
CRM_PK_ACCEL
C
typedef crm_pk_accel *(*FUNC_CRM_PK_POP_FINISHED_REQ)(struct crm_pk_cnx *cnx); #define CRM_PK_POP_FINISHED_REQ ((FUNC_CRM_PK_POP_FINISHED_REQ)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_POP_FINISHED_REQ)))
Description
Return the public key acceleration request which finished its operation. If no public key accelerator finished or none has an operation, return NULL. The results from the returned crm_pk_accel should be used as soon as possible and the instances given back with CRM_PK_RELEASE_REQ().
Parameters
| Param | Description |
|---|---|
| cnx | Connection structure obtained through CRM_PK_OPEN() at startup |
Returns
NULL when no public key accelerator finished The acceleration request which finished its operation
CRM_PK_GET_GLOBAL_NOTIFICATION_ID
C
typedef int (*FUNC_CRM_PK_GET_GLOBAL_NOTIFICATION_ID)(struct crm_pk_cnx *cnx); #define CRM_PK_GET_GLOBAL_NOTIFICATION_ID ((FUNC_CRM_PK_GET_GLOBAL_NOTIFICATION_ID)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_GET_GLOBAL_NOTIFICATION_ID)))
Description
Return a platform notification that notifies when a request completed. The platform notification id is:
- -1 if not available
- a fd on POSIX systems
- an interrupt line number
When a request completes the notification will activate. The fd will become readable and the interrupt line will generate an interrupt. The returned platform notification can be used once. After the platform notification or after CRM_PK_POP_FINISHED_REQ(), the notification id shall not be used anymore. May not be used in combination with CRM_PK_WAIT().
Parameters
| Param | Description |
|---|---|
| cnx | Connection structure obtained through CRM_PK_OPEN() at startup |
Returns
Platform notification id
CRM_PK_GET_REQ_COMPLETION_ID
C
typedef int (*FUNC_CRM_PK_GET_REQ_COMPLETION_ID)(crm_pk_accel *req); #define CRM_PK_GET_REQ_COMPLETION_ID ((FUNC_CRM_PK_GET_REQ_COMPLETION_ID)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_GET_REQ_COMPLETION_ID)))
Description
Return a platform notification that notifies when a request completed. The platform notification id is:
- -1 if not available
- a fd on POSIX systems
- an interrupt line number
When a request completes the notification will activate. The fd will become readable and the interrupt line will generate an interrupt.After it was used or after CRM_PK_POP_FINISHED_REQ(), the fd or interrupt line shall not be used anymore. May not be used in combination with CRM_PK_WAIT().
Parameters
| Param | Description |
|---|---|
| req | The acceleration request obtained through CRM_PK_ACQUIRE_REQ |
Returns
Platform notification id
CRM_PK_GET_OUTPUT_OPS
C
typedef const char **(*FUNC_CRM_PK_GET_OUTPUT_OPS)(crm_pk_accel *req); #define CRM_PK_GET_OUTPUT_OPS ((FUNC_CRM_PK_GET_OUTPUT_OPS)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_GET_OUTPUT_OPS)))
Description
Fetch array of addresses to output operands
Parameters
| Param | Description |
|---|---|
| req | The acceleration request obtained through CRM_PK_ACQUIRE_REQ |
Returns
Array of addresses to output operands
CRM_PK_RELEASE_REQ
C
typedef void (*FUNC_CRM_PK_RELEASE_REQ)(crm_pk_accel *req); #define CRM_PK_RELEASE_REQ ((FUNC_CRM_PK_RELEASE_REQ)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_PK_RELEASE_REQ)))
Description
Give back the public key acceleration request. Release the reserved resources
PRE
CRM_PK_ACQUIRE_REQ() should have been called before this function is called and not being in use by the hardware
Parameters
| Param | Description |
|---|---|
| req | The acceleration request obtained through CRM_PK_ACQUIRE_REQ() operation has finished |
Returns
None