CRM_CCM_IV_SZ
C
#define CRM_GCM_IV_SZ 12u
Description
Initialization vector (IV) size, in bytes, for GCM encryption/decryption
CRM_GCM_TAG_SZ
C
#define CRM_GCM_TAG_SZ 16u
Description
Size, in bytes, of GCM authentication tag
CRM_CCM_MAX_TAG_SZ
C
#define CRM_CCM_MAX_TAG_SZ 16u
Description
Maximum size, in bytes, of CCM authentication tag
CRM_AEAD_CREATE_AESGCM_ENC
C
typedef int (*FUNC_CRM_AEAD_CREATE_AESGCM_ENC)(struct crmaead *c, const struct crmkeyref *key, const char *iv); #define CRM_AEAD_CREATE_AESGCM_ENC ((FUNC_CRM_AEAD_CREATE_AESGCM_ENC)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_AEAD_CREATE_AESGCM_ENC)))
Description
Prepares an AES GCM AEAD encryption operation. This function initializes the user allocated object \p c with a new AEAD encryption operation context needed to run the AES GCM operation and reserves the HW resource. After successful execution of this function, the context \p c can be passed to any of the AEAD functions. pre - key reference provided by \p key must be initialized using CRM_KEYREF_LOAD_MATERIAL() or CRM_KEYREF_LOAD_BY_ID() remark - \p key and \p iv buffers should not be changed until the operation is completed. remark - GMAC is supported by using GCM with plaintext with size 0. remark - GCM and GMAC support AAD split in multiple chunks, using context saving.
Parameters
| Param | Description |
|---|---|
| c | AEAD operation context |
| key | key used for AEAD operation, expected size 16, 24 or 32 bytes |
| iv | Initialization vector, size must be 12 bytes |
Returns
CRM_OK CRM_ERR_INVALID_KEYREF CRM_ERR_INVALID_KEY_SZ CRM_ERR_INCOMPATIBLE_HW CRM_ERR_RETRY
CRM_AEAD_CREATE_AESGCM_DEC
C
typedef int (*FUNC_CRM_AEAD_CREATE_AESGCM_DEC)(struct crmaead *c, const struct crmkeyref *key, const char *iv); #define CRM_AEAD_CREATE_AESGCM_DEC ((FUNC_CRM_AEAD_CREATE_AESGCM_DEC)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_AEAD_CREATE_AESGCM_DEC)))
Description
Prepares an AES GCM AEAD decryption operation. This function initializes the user allocated object \p c with a new AEAD decryption operation context needed to run the AES GCM operation and reserves the HW resource. After successful execution of this function, the context \p c can be passed to any of the AEAD functions. @param c AEAD operation context @param key key used for the AEAD operation, expected size 16, 24 or 32 bytes @param iv initialization vector, size must be 12 bytes @pre - key reference provided by \p key must be initialized using CRM_KEYREF_LOAD_MATERIAL() or CRM_KEYREF_LOAD_BY_ID() @remark - \p key and \p iv buffers should not be changed until the operation is completed. @remark - GMAC is supported by using GCM with ciphertext with size 0. @remark - GCM and GMAC support AAD split in multiple chunks, using context saving.
Parameters
| Param | Description |
|---|---|
| c | AEAD operation context |
| key | key used for AEAD operation, expected size 16, 24 or 32 bytes |
| iv | Initialization vector, size must be 12 bytes |
Returns
CRM_OK CRM_ERR_INVALID_KEYREF CRM_ERR_INVALID_KEY_SZ CRM_ERR_INCOMPATIBLE_HW CRM_ERR_RETRY
CRM_AEAD_CREATE_AESCCM_ENC
C
typedef int (*FUNC_CRM_AEAD_CREATE_AESCCM_ENC)(struct crmaead *c, const struct crmkeyref *key, const char *nonce, size_t noncesz, size_t tagsz, size_t aadsz, size_t datasz); #define CRM_AEAD_CREATE_AESCCM_ENC ((FUNC_CRM_AEAD_CREATE_AESCCM_ENC)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_AEAD_CREATE_AESCCM_ENC)))
Description
Prepares an AES CCM AEAD encryption operation.
This function initializes the user allocated object \p c with a new AEAD encryption operation context needed to run the AES GCM operation and reserves the HW resource. After successful execution of this function, the context \p c can be passed to any of the AEAD functions. pre - key reference provided by \p key must be initialized using CRM_KEYREF_LOAD_MATERIAL() or CRM_KEYREF_LOAD_BY_ID() remark - the same aadsz and datasz must be provided to crm_aead_encrypt() or crm_aead_decrypt() functions. remark - \p key and \p nonce buffers should not be changed until the operation is completed. remark - CCM DOES NOT support AAD split in multiple chunks
Parameters
| Param | Description |
|---|---|
| c | AEAD operation context |
| key | key used for AEAD operation, expected size 16, 24 or 32 bytes |
| iv | Initialization vector, size must be 12 bytes |
Returns
CRM_OK CRM_ERR_INVALID_KEYREF CRM_ERR_INVALID_KEY_SZ CRM_ERR_INCOMPATIBLE_HW CRM_ERR_RETRY
CRM_AEAD_CREATE_AESCCM_DEC
C
typedef int (*FUNC_CRM_AEAD_CREATE_AESCCM_DEC)(struct crmaead *c, const struct crmkeyref *key, const char *nonce, size_t noncesz, size_t tagsz, size_t aadsz, size_t datasz); #define CRM_AEAD_CREATE_AESCCM_DEC ((FUNC_CRM_AEAD_CREATE_AESCCM_DEC)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_AEAD_CREATE_AESCCM_DEC)))
Description
Prepares an AES CCM AEAD decryption operation. This function initializes the user allocated object \p c with a new AEAD decryption operation context needed to run the AES GCM operation and reserves the HW resource. After successful execution of this function, the context \p c can be passed to any of the AEAD functions.
pre - key reference provided by \p key must be initialized using CRM_KEYREF_LOAD_MATERIAL() or CRM_KEYREF_LOAD_BY_ID() remark - the same aadsz and datasz must be provided to crm_aead_encrypt() or crm_aead_decrypt() functions. remark - \p key and \p nonce buffers should not be changed until the operation is completed. remark - CCM DOES NOT support AAD split in multiple chunks
Parameters
| Param | Description |
|---|---|
| c | AEAD operation context |
| key | key used for AEAD operation, expected size 16, 24 or 32 bytes |
| noncesz | size, in bytes, of the nonce, between 7 and 13 bytes |
| nonce | nonce used for the AEAD operation, with size \p noncesz |
| tagsz | size, in bytes, of the tag used for the AEAD operation, must be a value in {4, 6, 8, 10, 12, 14, 16} |
| aadsz | size, in bytes, of the additional authenticated data(AAD) |
| datasz | size, in bytes, of the data to be processed |
Returns
CRM_OK CRM_ERR_INVALID_KEYREF CRM_ERR_INVALID_KEY_SZ CRM_ERR_INCOMPATIBLE_HW CRM_ERR_RETRY
CRM_AEAD_FEED_AAD
C
typedef int (*FUNC_CRM_AEAD_FEED_AAD)(struct crmaead *c, const char *aad, size_t aadsz); #define CRM_AEAD_FEED_AAD ((FUNC_CRM_AEAD_FEED_AAD)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_AEAD_FEED_AAD)))
Description
Adds AAD chunks
This function is used for adding AAD buffer given by \p aad. The function will return immediately. pre - one of the crm_aead_create_*() functions must be called first remark - the additional authentication data can be empty(\p aadsz = 0) remark - \p aad buffer should not be changed until the operation is completed.
Parameters
| Param | Description |
|---|---|
| c | AEAD operation context |
| aad | additional authentication data(AAD), with size \p addsz |
| aadsz | size, in bytes, of the additional authenticated data(AAD), can be 0 if \p aad is empty |
Returns
CRM_OK CRM_ERR_UNINTIALIZED_OBJ CRM_ERR_TOO_BIG
CRM_AEAD_CRYPT
C
typedef int (*FUNC_CRM_AEAD_CRYPT)(struct crmaead *c, const char *datain, size_t datainsz, char *dataout); #define CRM_AEAD_CRYPT ((FUNC_CRM_AEAD_CRYPT)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_AEAD_CRYPT)))
Description
Adds data to be encrypted or decrypted.
This function is used for adding data to be processed. The function will return immediately. The result of the operation will be transfered to \p dataout after the operation is successfully completed.
For context saving, \p datain size(\p datainsz) must be a multiple of 16 bytes for AES GCM and CCM and a multiple of 64 bytes for ChaCha20Poly1305, except the last buffer. remark - \p datain buffer should not be changed until the operation is completed.
Parameters
| Param | Description |
|---|---|
| c | AEAD operation context |
| datainsz | size, in bytes, of the data to be encrypted or decrypted |
| datain | data to be encrypted or decryoted, with size \p datainsz |
| dataout | dataout encrypted or decrypted data, must have \p datainsz bytes |
Returns
CRM_OK CRM_ERR_UNINTIALIZED_OBJ CRM_ERR_TOO_BIG
CRM_AEAD_PRODUCE_TAG
C
typedef int (*FUNC_CRM_AEAD_PRODUCE_TAG)(struct crmaead *c, char *tagout); #define CRM_AEAD_PRODUCE_TAG ((FUNC_CRM_AEAD_PRODUCE_TAG)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_AEAD_PRODUCE_TAG)))
Description
Starts an AEAD encryption and tag computation.
The function will return immediately.
The computed tag will be transfered to \p tag only after the operation is successfully completed.
The user shall check operation status with crm_aead_status() or CRM_AEAD_WAIT().
pre - one of the CRM_AEAD_FEED_AAD() or CRM_AEAD_CRYPT() functions must be called first
remark - if used with context saving(last chunk), the fed data size for the last chunk can not be 0
Parameters
| Param | Description |
|---|---|
| c | AEAD operation context |
| tag | authentication tag |
Returns
CRM_OK CRM_ERR_UNINTIALIZED_OBJ CRM_ERR_TOO_BIG
CRM_AEAD_VERIFY_TAG
C
typedef int (*FUNC_CRM_AEAD_VERIFY_TAG)(struct crmaead *c, const char *tagin); #define CRM_AEAD_VERIFY_TAG ((FUNC_CRM_AEAD_VERIFY_TAG)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_AEAD_VERIFY_TAG)))
Description
Starts an AEAD decryption and tag validation. The function will return immediately. The user shall check operation status with crm_aead_status() or CRM_AEAD_WAIT(). pre - one of the CRM_AEAD_FEED_AAD() or CRM_AEAD_CRYPT() functions must be called first remark - \p tag buffer should not be changed until the operation is completed. remark - if used with context saving(last chunk), the fed data size for the last chunk can not be 0
Parameters
| Param | Description |
|---|---|
| c | AEAD operation context |
| tag | authentication tag |
Returns
CRM_OK CRM_ERR_UNINTIALIZED_OBJ CRM_ERR_TOO_BIG
CRM_AEAD_RESUME_STATE
C
typedef int (*FUNC_CRM_AEAD_RESUME_STATE)(struct crmaead *c); #define CRM_AEAD_RESUME_STATE ((FUNC_CRM_AEAD_RESUME_STATE)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_AEAD_RESUME_STATE)))
Description
Resumes AEAD operation in context-saving.
This function shall be called when using context-saving to load the state that was previously saved by crm_aead_save_state() in the crmaead operation context \p c. It must be called with the same crmaead operation context \p c that was used with crm_aead_save_state(). It will reserve all hardware resources required to run the partial AEAD operation. Previously used mode and direction are already stored in crmaead \p c.
After successful execution of this function, the context \p c can be passed to any of the AEAD functions, except the crm_aead_create_() functions. pre - crm_aead_create_aes() and crm_aead_save_state() functions must be called before, for first part of the message. pre - must be called for each part of the message(besides first), before CRM_AEAD_CRYPT() or crm_aead_save_state().
remark - the user must not change the key until all parts of the message to be encrypted/decrypted are processed.
Parameters
| Param | Description |
|---|---|
| c | AEAD operation context |
Returns
CRM_OK CRM_ERR_UNITIALIZED_OBJ CRM_ERR_CONTEXT_SAVING_NOT_SUPPORTED CRM_ERR_INVALID_KEYREF CRM_ERR_INVALID_KEY_SZ CRM_ERR_INCOMPATIBLE_HW CRM_ERR_RETRY
CRM_AEAD_SAVE_STATE
C
typedef int (*FUNC_CRM_AEAD_SAVE_STATE)(struct crmaead *c); #define CRM_AEAD_SAVE_STATE ((FUNC_CRM_AEAD_SAVE_STATE)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_AEAD_SAVE_STATE)))
Description
Starts a partial AEAD operation. This function is used to start a partial encryption or decryption of \p datain. The function will return immediately.
The partial result will be transfered to \p dataout only after the operation is successfully completed. The user shall check operation status with crm_aead_status() or CRM_AEAD_WAIT(). pre - CRM_AEAD_CRYPT() should be called first. remark - the user must not change the key until all parts of the message to be encrypted/decrypted are processed. remark - when in context saving, the sizes of the chunks fed must be multiple of 16 bytes, besides the last chunk that can be any size, but not 0
Parameters
| Param | Description |
|---|---|
| c | AEAD operation context |
Returns
CRM_OK CRM_ERR_UNITIALIZED_OBJ CRM_ERR_CONTEXT_SAVING_NOT_SUPPORTED CRM_ERR_WRONG_SIZE_GRANULARITY
CRM_AEAD_WAIT
C
typedef int (*FUNC_CRM_AEAD_WAIT)(struct crmaead *c); #define CRM_AEAD_WAIT ((FUNC_CRM_AEAD_WAIT)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_AEAD_WAIT)))
Description
Waits until the given AEAD operation has finished
This function returns when the AEAD operation was successfully completed, or when an error has occurred that caused the operation to terminate. The return value of this function is the operation status. After this call, all resources have been released and \p c cannot be used again unless crm_aead_create_() is used. making \p c unusable for a new operation without calling, first, one of the crm_aead_create_() functions. pre - crm_aead_encrypt or crm_aead_decrypt() function must be called first remark - this function is blocking until operation finishes.
Parameters
| Param | Description |
|---|---|
| c | AEAD operation context |
See
crm_aead_status()
Returns
CRM_OK CRM_ERR_UNITIALIZED_OBJ CRM_ERR_DMA_FAILED CRM_ERR_INVALID_TAG
CRM_AEAD_STATUS
C
typedef int (*FUNC_CRM_AEAD_STATUS)(struct crmaead *c); #define CRM_AEAD_STATUS ((FUNC_CRM_AEAD_STATUS)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_AEAD_STATUS)))
Description
Returns the AEAD operation status.
If the operation is still ongoing, return ::CRM_ERR_HW_PROCESSING. In that case, the user can retry later.
When this function returns with a code different than ::CRM_ERR_HW_PROCESSING, the AEAD operation has ended and all resources used by the AEAD operation context \p c have been released. In this case, \p c cannot be used for a new operation until one of the crm_aead_create_*() functions is called again.
pre - crm_aead_encrypt or crm_aead_decrypt() function must be called first
remark - if authentication fails during decryption, ::CRM_ERR_INVALID_TAG will be returned. In this case, the decrypted text is not valid and shall not be used.
Parameters
| Param | Description |
|---|---|
| c | AEAD operation context |
See
crm_aead_status()
Returns
CRM_OK CRM_ERR_UNITIALIZED_OBJ CRM_ERR_HW_PROCESSING CRM_ERR_DMA_FAILED CRM_ERR_INVALID_TAG