CRM_MAC_CREATE_AESCMAC
C
typedef int (*FUNC_CRM_MAC_CREATE_AESCMAC)(struct crmmac *c, const struct crmkeyref *key); #define CRM_MAC_CREATE_AESCMAC ((FUNC_CRM_MAC_CREATE_AESCMAC)(*(uint32_t *)(API_TABLE_BASE_ADDRESS + ATO_CRM_MAC_CREATE_AESCMAC)))
Description
Prepares an AES CMAC generation.
This function initializes the user allocated object \p c with a new AES CMAC operation context needed to run the CMAC generation. After successful execution of this function, the context \p c can be passed to any of the CMAC functions. @pre - key reference provided by \p key must be initialized using CRM_KEYREF_LOAD_MATERIAL() or CRM_KEYREF_LOAD_BY_ID()
Parameters
| Param | Description |
|---|---|
| c | CMAC operation context |
| key | Key used for the CMAC generation operation, expected size 16, 24 or 32 bytes |
Returns
CRM_OK CRM_ERR_INVALID_KEYREF CRM_ERR_INVALID_KEY_SZ CRM_ERR_INCOMPATIBLE_HW CRM_ERR_RETRY