1.1 ADC Automatic Window Comparison
This example application shows how to sample an analog input in polled mode and send the converted data to console using automatic window comparison of converted values.
Description
This example application shows how to use the ADC Peripheral library to perform automatic window comparison of converted values.
The ADC peripheral is configured to operate in window mode. In this example, Analog input voltage in the range of 0V to 3.3V is fed to the ADC input channel AD6. The ADC conversion is triggered by software and converted result is displayed on the console whenever input voltage goes below window lower threshold.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/adc/adc_automatic_window_comparison/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_9x75_curiosity.X | MPLAB project for SAM9X75 Curiosity Development Board |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, the user needs to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_9x75_curiosity.X | SAM9X75 Curiosity Development Board |
Setting Up SAM9X75 Curiosity Development Board
- Connect the UART DEBUG J35 on board to the computer using a UART-FTDI cable (to enable debug com port)
- Connect the USB port J2 on board to the computer using a micro USB cable (to power the board)
- Use a jumper wire to connect Pin TX of mikroBUS (AD4 is mapped to Port Pin PA28) to 3.3V or GND (OR Use Potentiometer to vary input voltage from GND to 3.3V and vice versa)
Running the Application
- Build the application using its IDE
- Open the Terminal application (Ex.:Tera term) on the computer
- Connect to the (USB to Serial) COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Console displays ADC Count and
ADC Input Voltage whenever input voltage goes below lower window threshold value
(output is not updated on console, if the values are within the threshold)
Note: Image provided in above step is for illustration purpose only. ADC count and ADC Input voltage are printed on the console whenever input voltage goes below 2.417V ((3000/4095) * 3.3V).