1.6 FAT Filesystem using AT24 EEPROM Media
This application shows an example of using the MPLAB Harmony File System to access I2C EEPROM based media.
Description
File System Operations on the On-Board SQI Flash Memory:
- Performs a SYS-FS_FormatDisk
- Opens a newfile.txt on the I2C EEPROM media (AT24 EEPROM)
- Write and reads back 4KB of data on newfile.txt
- Verifies the Data Read back
File system layer uses:
- Memory driver to communicate with external AT24 EEPROM device using I2C
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/fs/i2c_eeprom_fat/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_e54_xpro.X | MPLABX project for SAM E54 Xplained Pro Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_e54_xpro.X | SAM E54 Xplained Pro Evaluation Kit |
Setting Up SAM E54 Xplained Pro Evaluation Kit
- To run the demo, the following additional hardware are required:
- Install an EEPROM 3 CLICK on to the mikroBUS Xplained Pro board
- Connect the mikroBUS Xplained Pro board to the EXT2 header
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Build and program the application using its IDE
- Press switch to start the operation
- The LED is turned ON if writing and reading is successful on EEPROM media
Refer to the following table for Switch and LED names:
| Board | Switch Name | LED Name |
|---|---|---|
| SAM E54 Xplained Pro Evaluation Kit | SW0 | LED0 |