1 Harmony 3 Peripheral Library Application Examples for PIC32MK Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more peripheral libraries.
| Name | Description |
|---|---|
| ADCHS DMA | This example application shows how to sample an analog input using the ADCHS peripheral in DMA mode and displays the converted samples on a serial terminal |
| ADCHS Interrupt | This example application shows how to sample an analog input using the ADCHS peripheral and displays the converted samples on a serial terminal |
| ADCHS Polling | This example application shows how to sample an analog input using the ADCHS peripheral and displays the converted samples on a serial terminal |
| CAN Blocking | This example application shows how to use the CAN module to transmit and receive normal CAN messages in polling mode |
| CAN FD Blocking | This example application shows how to use the CAN module to transmit and receive CAN FD messages in polling mode |
| CAN FD Interrupt | This example application shows how to use the CAN module to transmit and receive CAN FD messages in interrupt mode |
| CAN Interrupt | This example application shows how to use the CAN module to transmit and receive normal CAN messages in interrupt mode |
| CDAC Waveform Generation | This example application shows how to use the CDAC to generate a 1 kHz sinusoidal waveform |
| CDAC Waveform Generation with DMA | This example application shows how to use the CDAC with the DMA to generate a 1 kHz sinusoidal waveform without CPU intervention |
| Clock Configuration | This example application shows how to configure the clock system to run the device at maximum frequency. It also outputs a prescaled clock signal on a GPIO pin for measurement and verification |
| CORETIMER Periodic Interrupt | This example application shows how to use the CoreTimer to generate periodic interrupts |
| DMAC Memory Transfer | This example application demonstrates how to use the DMAC peripheral to do a memory to memory transfer |
| EEPROM Read Write | This example application demonstrates how to use the EEPROM peripheral library |
| GPIO Interrupt | This example application demonstrate how to generate GPIO interrupt on switch press and release, and indicate the switch status using the LED |
| GPIO Polling | This example application demonstrate how to poll the switch input, and indicate the switch status using the LED |
| I2C EEPROM Read Write | This example application demonstrates how to use the I2C peripheral to write and read from the I2C serial EEPROM memory |
| I2C SMBUS read write | This example application demonstrates how to use the I2C peripheral to exchange data between a device acting as a SMBUS master and SMBUS slave. |
| I2C Temperature Sensor | This example application demonstrates how to use I2C peripheral to read temperature value from temperature sensor device |
| ICAP Capture Mode | This example application shows how to use the ICAP peripheral to measure the pulse width of the input signal |
| MCPWM Channels | This example demonstrates how to use the MCPWM peripheral to generate PWM signals |
| NVM Flash Read Write | This example application demonstrates how to use the NVM to erase and program the internal Flash memory |
| OCMP Compare Mode | This example application shows how to use the OCMP peripheral to generate an active low, active high, and toggle output on compare match |
| RTCC Alarm Interrupt | This example application shows how to use the RTCC to configure the time and generate the alarm |
| SPI Blocking | This example application demonstrates how to use the SPI peripheral to transmit and receive a block of data in a blocking manner |
| SPI EEPROM Write Read | This example application demonstrates how to use the SPI peripheral to write and read from the SPI serial EEPROM memory |
| SPI Interrupt | This example application demonstrates how to use the SPI peripheral to transmit and receive a block of data using interrupt |
| SPI Host Read Write Test Application | This is a SPI Host test application which is provided to demonstrate communication between SPI host and the corresponding SPI client application available under - apps/spi/slave/spi_write_read/firmware |
| SPI Client Read Write | This example application demonstrates how to use the SPI peripheral in client mode |
| TMR Periodic Interrupt | This example demonstrates how to use the TMR module in timer mode to generate periodic interrupt |
| TMR1 Periodic Interrupt | This example demonstrates how to use the TMR1 module in timer mode to generate periodic interrupt |
| UART Auto-baud | This example application demonstrates how to use auto-baud feature of UART peripheral |
| UART Echo Blocking | This example application demonstrates how to use the UART peripheral to transfer a block of data in a blocking manner |
| UART Echo Interrupt | This example application demonstrates how to use the UART peripheral to transfer a block of data in a non-blocking manner |
| UART Ring Buffer | This example application demonstrates how to use the UART peripheral in ring buffer mode |
| WDT Timeout | This example application shows how the watchdog timer resets by not feeding the watchdog on switch press |