12 Known Issues and Limitations
(Ask a Question)This section lists Libero SoC Design Suite known issues and limitations.
12.1 Libero
(Ask a Question)The following table lists the known issues and limitations associated with Libero.
| Family | Description | Version Identified | Version Fixed | Status |
|---|---|---|---|---|
| All | On Ubuntu® 20.04.6 LTS, the following error
message appears when launching
Libero:This
error also occurs in the following scenarios:
While a few cores may download successfully, the majority of downloads fail due to this error. Workaround: Run the following commands as
| 2025.1 | Open | |
| PolarFire and PolarFire SoC | I/O Bank Setting does not reflect available I/O standards correctly for mixed voltage I/Os. Workaround: Check I/O Editor's Port View and confirm that appropriate I/O standards are assigned based on Mixed voltage I/O standard assignments. For additional information, see Article Number 000016039. | 12.5 | Open | |
| All | After executing the
download_latest_core command without an internet connection, a
message indicates that all cores are up to date. It is important to inform you when
there is an issue with your internet connection. | 2022.2 | 2025.1 | Fixed |
| RTG4 |
When creating and configuring the RTG4 INIT cores (NPSS_SERDES_IF_INIT,
PCIE_SERDES_IF_INIT, and RTG4FDDR_INIT) and SmartFusion2/IGLOO2 System Builder
cores, trying to generate the components by calling the TCL command
Workaround: Instead of importing a previously configured IP catalog core component (.CXF plus
.SDB) and generating the component using the
Note: If the core is already created and needs only regeneration, remove the
create_and_configure_core command from the exported script
file. | 2023.2 | Open | |
| PolarFire and PolarFire SoC | If you use BIBUF_DIFF or TRIBUFF_DIFF in your design and set the default IOSTD to be LVCMOS33, these I/Os will take the LVDS33 IOSTD by default, which is not supported. Workaround: The best practice is to set the IOSTD for each I/O explicitly in the PDC file. Do not use the LVCMOS33 IOSTD as a default when BIBUF_DIFF or TRIBUFF_DIFF is in your design. | 12.0 | N/A | Open |
| RTG4 | A corner case existed where a CLKINT was instantiated with its input tied to a static '1' and then routed using only a half-chip Global Buffer (GBL or GBR). A user signal routed on the corresponding other half GB might be output from the CLKINT tied to a static '1'. Workaround: In the unlikely event that a CLKINT has been instantiated and tied to a static
| 11.6 | 2024.1 | Fixed |
| RTG4 | Instantiating the RTG4_ODT_DYN macro for an I/O bank causes Libero SoC to mark three extra I/Os
on that bank as User Reserved and physically configure them as unused
I/O. The three I/O pins reserved are always the same for a given I/O bank, as
shown below: If the design requires assigning a user signal to any of these reserved pins when RTG4_ODT_DYN is instantiated, upgrade to Libero SoC v2024.1 or later. | 12.0 | 2024.1 | Fixed |
| All | The Memory Map report does not appear correctly if the AHBL_READ_INITIATOR and AHBL_WRITE_INITIATOR pins are exposed in the MIV_ESS v2.0.100 core. | 2024.1 | ||
| IGLOO2, SmartFusion2, RTG4, PolarFire, PolarFire SoC | If the Synthesis step is bypassed in the Design Flow
project settings, block components published with VHDL language mode enabled may
fail to compile when instantiated in the top-level project. If this occurs, the
compile step reports the following
error:Workaround:
Publish all block components with Libero project settings set to Verilog language.
Alternatively, re-run Synthesis on the top-level project so that a mapped Verilog
(.vm) is used during Compile. | 12.0 | N/A | Will not fix |
| PolarFire | Multipass Place and Route intermittently
reportsThe
mutlipass Place and Route run completes successfully, and the best result is saved
into the project. However, the summary table showing the results across all seeds
is not displayed. Note: This issue does not occur for all starting seed indexes in the Place and
Route options.
| 2022.3 | 2024.2 | Fixed |
| PolarFire | The memory map functionality (exporting Memory Map or viewing it in SmartDesign) is not supported for the MIV_ESS v2.0.200 core. | 2024.1 | Open | |
All | If an MSS or MiV processor interrupt pin is connected to a 1-bit slice pin through a connection hierarchy, incorrect information might appear in the exported Interrupt Map Report file. Workaround: If the Interrupt Map Report is not correct for your design, replace the one-bit slices with regular scalar connections when entering or exiting the hierarchy. | 2023.1 | 2023.2 | Fixed |
PolarFire SoC | If you set the default I/O standard to 2.5V (which sets
the bank voltage of the I/Os to 2.5V automatically) in the Libero project setting,
assigning MSS I/O Bank voltage to 3.3V (that is, VCCI =3.3V) using PDC constraint
generates following error
message:Workaround:
Change the default I/O standard in Libero project setting to LVCMOS33 or LVTTL and
update other I/Os to accommodate the change. | 2022.1 | Open | |
PolarFire, PolarFire SoC | PF_CCC: PLL outputs are not phase aligned consistently after multiple Power Cycle/toggling of the powerdown pin. | 2021.1 | 2022.2 | Fixed |
| RTG4 | If the RTG4FCCCECALIB core is configured for external feedback mode with FB_CLK sourced from a CCC GLx output, and if the CCC outputs are configured to remain low until PLL lock is acquired, a deadlock condition occurs because the FB_CLK input never toggles, preventing the PLL from locking. If external feedback is selected in the standard RTG4FCCC core, Libero ignores the user option to hold CCC outputs low until the PLL locks to prevent such a deadlock. The RTG4FCCCECALIB core will be updated in a future release to remove the deadlock condition by ignoring the option to hold CCC outputs low when external feedback is selected. Workaround: If using external feedback mode, allow the CCC outputs to operate even before PLL lock is acquired (default). Alternatively, edit the generated RTG4FCCCECALIB core HDL manually so that the GL#_Y#_EN input to the CCC primitive is tied to ‘1’ for the CCC GLx output used to drive the FB_CLK input. | 2021.3 | 2022.2 | Fixed |
| RT PolarFire, PolarFire | RT PolarFire, MPF500T: Design contains encrypted blocks and Synthesis (or Compile) fails with the following message.Possible reasons:
| 2021.3 | 2022.3 | Fixed |
| All | If there is no MSS or a MiV processor in a SmartDesign, exporting an interrupt map report causes Libero to crash. | 2022.3 | 2023.1 | Fixed |
| All | If two different VHDL files have the same signature (same inputs, outputs, and architecture), the modules are not detected as duplicate modules in the Design Hierarchy. | 12.4 | Open | |
| All | If a module is present in an include file, the file
appears as a linked file inside the project. If there is a broken Global Include
Path for such projects, the include file is also shown with a broken link. If the
project is closed and re-created, the correct Global Include Path appears properly.
If the Global Include path under Project Settings is changed,
two links are shown for the include file inside the project:
| 12.5 | Open | |
| All | Linux CentOS7.9 UI test: Users cannot view help topics. Workaround: In Firefox, go to and change the value to False. Then reopen the help. | 2022.1 | N/A | Will not fix |
| PolarFire and PolarFire SoC | In , Libero 2022.3 users who check Enable FPGA Hardware
Breakpoint Auto Instantiation and then hover over the
i near the GUI option should ignore the following message
that appears beside the FHB check mark because the new FHB compile implementation
allows the FHB to be instantiated on any CLKINTs:
| 2022.3 | 2023.1 | Fixed |
| PolarFire and PolarFire SoC | Incorrect PUFT timing is reported when SPI Flash uses an Initialization client. | 2021.2 | N/A | Will not fix |
| PolarFire and PolarFire SoC | To invoke FHB auto-instantiation flows with PolarFire and PolarFire SoC, you must create your own NDC file using auto_instantiate_fhb commands. If the NDC file is named with the postfix fhb_auto_generated.ndc, the flow deletes the file and crashes. Workaround: Do not name or use files with the postfix fhb_auto_generated.ndc when using FHB auto-instantiation flows in PolarFire and PolarFire SoC. | 2022.3 | 2023.1 | Fixed |
| RTG4, PolarFire, and PolarFire SoC | I/O Editor shows resistor pull for P and N pins when LVDS failsafe (Dynamic ODT) is enabled. For RTG4, PolarFire, and PolarFire SoC families, the resistor pull information for P and N pins are shown as pull up or both as pull down. They should be pull up for one pin and pull down for the other pin. This is a display issue only that existed in the I/O Editor and the pin report since v11.9 SP3. Due to a software infrastructure limitation, the P and N sides cannot have different values. Regardless of the display issue, both P and N sides program correctly:
| 12.4 | Open | |
| RTG4 | In the PLL Options tab under Output Resynchronization After Lock, when the option Held output in reset (output low) after power-up. Released and resynchronized with the PLL reference clock after the PLL locked is set for the RTG4FCCCECALIB core, the output clock appears at the CCC output slightly before the LOCK output is asserted. Workaround: When synchronizer is used for the LOCK signal, do not use the GLx output clock. For example, use the free-running clock CLK_50 MHz to clock the synchronizer circuit. Use the output of the three-stage synchronizer to drive both the LOCK signal and the GLx_Yx_EN signal. For more information, see the RTG4 FCCC Enhanced PLL Calibration Configurator User Guide . | 2021.2 | Open | |
| PolarFire and PolarFire SoC | A new FHB implementation allows FHBs to be added to any CLKINT/RCLKINT/GCLKINT/RGCLKINT of a design. However, there are some limitations about the kind of topologies allowed. With SmartBERT, the RCLKINTs connected to output RX_CLK_R and TX_CLK_R are considered illegal instances for FHB instantiation. These instances are considered to be illegal because FHB instantiations create an additional CLKINT and connect it to the same driver as the RCLKINT; however, the RX_CLK_R and TX_CLK_R nets are considered dedicated lines and allow only one connection. As a result, the additional CLKINT cannot make the connection and causes the flows to error-out. | 2022.3 | 2023.1 | Fixed |
12.2 Synthesis/Simulation
(Ask a Question)The following table lists the known issues and limitations associated with Synthesis/Simulation.
| Family | Description | Version Identified | Version Fixed | Status |
|---|---|---|---|---|
| All | The Libero SoC tool is unable to recognize Synopsys all-vendor tools such as Synplify Elite and Synplify Apex, starting with Synplify version T-2022.09. As a result, synthesis fails when these tools are selected from in Libero SoC version 2023.1 and later. Workaround: None | 2023.1 | 2025.1 | Fixed |
| All | If your RTL includes complex index conversion functions, such as
The crash occurs due to a problem with constant optimization. The use of conversion functions,
such as Workaround: To resolve the issue, modify the RTL by relocating the more complex index computation expression outside of the index expression, as demonstrated below: Original RTL Causing Crash:
Workaround RTL:
| 11.9 | N/A | Open |
| All | The Synplify TMR report does not report arch-level TMR. Workaround: The SynplifyPro tool performs the TMR implementation accurately. However, the TMR report is not generated correctly. The TMR implementation can be confirmed either by referring to the *.srr log file or examining the generated VM netlist. | 2022.1 | 2024.1 | Fixed |
| RTG4 | If a module from one VHDL file instantiates another module defined in a different VHDL file located in a separate library, the Stimulus Hierarchy may not display correctly. Additionally, if the same VHDL modules are defined in multiple VHDL libraries, the hierarchies may not build correctly and a "?" might be shown for modules are that are not found. Workaround: If the Design Hierarchy is not correctly understood by the tool, either re-organize the way the VHDL modules and libraries are defined to avoid the scenario described, or right-click the Synthesize step in the design flow to select , and then create a manual file organization by telling Libero SoC which source files should be used for Synthesis and in which order. | 2022.1 | Open | |
| SmartFusion2 | The SmartFusion2 MSS DDR Fabric Interface Controller (FIC) AXI port exhibits incorrect read channel behavior during simulation. If the read address channel operates independently from the read data response channel, it can lead to incorrect ARREADY behavior. Additionally, depending on the clock ratio between the DDR and fabric interfaces, misaligned read data may occur on the fabric AXI bus. Workaround: Please contact Microchip Technical Support to request pre-compiled libraries tailored to your specific simulator to address this issue. Kindly refer to Case Number 01019123. | 2022.1 | Open | |
| All | Synplify Pro versions S-2021.09-SP2, S-2021.09M, and S-2021.09M-SP1 can incorrectly synthesize Verilog RTL using increment/decrement operations (++ / --) while indexing into an array on the right-hand side (RHS) of an assignment statement. Workaround: The Verilog can be modified to perform the increment/decrement operation in a for loop instead of during array indexing Note: For additional details, see PCN BLAS-18JFVA747. | 2022.1 | 2022.3 | Fixed |
| All | Prior to Synplify Pro ME version S-2021.09M-SP2 and all-vendor version T-2022.09, Synplify Pro synthesis software could incorrectly implement VHDL expressions containing a subtraction with a real constant number operand, and an additional division/multiplication operation that uses a variable. The issue occurs when the division/multiplication using a variable occurs in either the minuend or subtrahend terms of the subtraction operation. Workaround: Upgrade the synthesis tools and re-synthesize the design using Synplify Pro ME version S-2021.09M-SP2, or Synplify Pro standalone version T-2022.09, or later. Note: For additional details, see PCN RMES-14NRSU939. | All | 2022.3 | Fixed |
| PolarFire, PolarFire SoC | Simulating encrypted IP CORE10GMAC designs with QuestaSim ME Pro 2023.1 optimizes the design in a way that causes the APB interface PREADY signal to go undefined. Workaround: Disable the optimization in encrypted code by adding the
| 2023.2 | Open | |
All | Siemens does not support ModelSim Windows 10 on I7-11th generation machine. | 2022.1 | N/A | Will not fix |
PolarFire | If automatic compile point is enabled, synthesis passes successfully, but Place and Route errors-out and points to the derived constraint file:
Workaround: Perform one of the following steps:
get_pins instead of get_nets)set_false_path
-through [ get_pins { AXI4_Interconnect_0/ARESETN* } ] | 12.9 | N/A | Will not fix |
N/A | Identify debugger 2021-03M with Libero 2021.2 crashes on 11th generation Windows 10 machines. | 2021.2 | 2022.1 | Fixed |
All | The vdir command used with ModelSim ME Pro 2021.3 for pre-compiled libraries on tess delivers the incorrect result of unknown version. | 2021.3 | 2022.2 | Fixed |
| All | In a Libero flow, when multiple identify implementations
are created and run initially, an error message appears only in the synthesis log and
does not propagate to the Libero error log. The following error message appears in the
Libero window:
| 2021.2 | Open | |
| All | If an Identify implementation was created through a Libero project before another synthesis implementation (synthesis_1) is created using , the next run synthesis_1 command fails. Checking the Active implementation dialog, confirming that there is no implementation in the pull-down menu, and then rerunning the Libero project places Libero in an unexpected stage. Workaround: When Identify implementation is created using , open SynplifyPro interactively, instrument the design, and run synthesis before running any synthesis or creating new implementation. Then return to Libero and create a new synthesis/identify implementation. | 2021.2 | Open | |
| All | With the SynplifyPro R2021.03M release, when Synplfiy Pro is invoked on the Ubuntu platform, it lists packages/libraries on the terminal. This message can be safely ignored. Similarly, choosing lists packages/libraries on the Ubuntu platform. When prompted, click OK to proceed. | 2021.2 | Open | |
| All | If multiple implementations are created in Libero/Synplify flows, rerun synthesis each time the active implementation is switched to have Libero fetch the intended .vm netlist for active implementation. | 2021.2 | Open | |
| PolarFire | The following enhancement to Synthesis Compiler in this SynplfiyPro 2020.09MSp1 release (Libero v2021.1 release) is related to the initial value support for memory initialization. This is not technology specific. Test cases with MiV core fails in synthesis with following error message: @E: Workaround: In the Libero GUI, select box and set the -looplimit option to 4000. OR Add the following
| 2021.1 | Open | |
| PolarFire | A low data rate of 500Mbps/250Mhz fails with the QDR II + Xtreme device in simulation, but passes on the board. | 2021.1 | Open |
12.3 Timing/Power
(Ask a Question)The following table lists the known issues and limitations associated with Timing/Power.
| Family | Description | Version Identified | Version Fixed | Status |
|---|---|---|---|---|
| IGLOO2, SmartFusion2 | SmartFusion2 (M2S150) and IGLOO2 (M2GL150) designs using clocks routed to the global network through RCLKINT macros may experience a skew-induced timing violation that is not reported during Static Timing Analysis. This issue can occur when multiple Row Global Buffers (RGBs) are cascaded to reach loads spanning a large FPGA fabric area per Customer Notification 19024.2. Workaround: Upgrade to Libero SoC v12.2 or later. For M2S150/M2GL150 designs already in production, contact Microchip Technical Support to obtain the timing analysis script referenced in CN19024.2 | 11.8 | 12.2 | Fixed Note: Fixed in Libero SoC v12.2 onwards. Not fixed in Libero SoC v11.x branch. |
| All | When writing SDC timing exceptions, such as false path, multicycle path, or set max/min delay
constraints, using the [get_clocks {…}] construct applies the
timing exception on the clock domain’s register-to-register
paths only, and not to the clock domain’s paths related to
inputs or outputs with associated set_input_delay or
set_output_delay constraints, respectively. For example, false
path constraints set between clock objects referenced using
Workaround: Avoid using | Libero IDE v8.0 | 2025.1 | Fixed |
| SmartFusion2 | The clock constraints generated by the software for oscillators internal to SmartFusion2 and Igloo2 devices use the oscillator typical clock period and not their worst case. Workaround: You can override these clock constraints using the worst-case period listed in the datasheet. | 12.4 | Open | |
| RTG4 | Libero SoC’s Verify Timing design flow step reports a timing violation in the multi-corner timing reports and Timing Report Explorer tabs. However, when opening the SmartTime GUI, the violation cannot be seen, even after confirming that SmartTime analysis operating conditions have been set to match the conditions used to identify the violation in the Verify Timing reports. The SmartTime GUI has an issue where the path list does not correctly account for the clock generation delay, even though the expanded path detail correctly accounts for the clock generation delay. Workaround: Always use the multi-corner timing violation reports to determine if there are timing violations. Use the Timing Report Explorer to review the violating path list graphically, until the SmartTime GUI issue is fixed. | 2024.1 | 2025.1 | Fixed |
| RTG4 | You might encounter errors during Net Delay Calculation when running Place and Route or Timing Verification if starting a Libero SoC project with an EDIF (.edn) netlist as the design source file. Workaround: Use the Synplify Pro mapped Verilog netlist (.vm file) as the source file instead of the EDIF (.edn) netlist. | 2023.1 | N/A | Will not fix |
| PolarFire SoC | TGrade2 for the MPFS460 devices is not supported. Remove the following parts from the software: MPFS460T-1FCG1152_EvalT2 MPFS460T-FCG1152_EvalT2 | 2021.3 | 2024.1 | Fixed |
| RTG4 | If a generated clock constraint is set on an unused CCC output, SDC processing fails during timing analysis and all following constraints are ignored. Workaround: Use derived constraints. | 2023.2 | N/A | Will not fix |
| RTG4 | Errors on clock names for
set_input_jitter are not reported.
set_input_jitter constraints with erroneous
clock names are simply ignored. | 2023.2 | 2024.1 | Fixed |
PolarFire and PolarFire SoC | Prior to Libero SoC v2023.2, designs targeting MPFS025xx and MPFS025xx devices could have placed High-Speed I/O Clock (HS_IO_CLK) instances at locations that are not routable. Required Action: Microchip recommends upgrading to Libero SoC v2023.2 and re-running Place and Route to ensure that HS_IO_CLK instances are not placed in non-routable locations | 2021.3 | 2023.2 | Fixed |
| PolarFire SoC | An MPFS160 design with a connection between an HS_IO_CLK and an ICB may fail during timing analysis with the following error message:
Workaround: Move the HS_IO_CLK to the next available location | 2023.1 | 2023.2 | Fixed |
| SmartFusion 2 | Cell delay for RAM1K18 IP in Clock-to-Output paths. | 2022.1 | 2022.3 | Fixed |
| All | The SSN Analyzer tool does not sort pins properly when determining I/O adjacency, resulting in the SSO analysis being incorrect. For RTG4, PolarFire, PolarFire SoC, and RT PolarFire, adjacent pin number sorting should be done by I/O pair number per I/O bank using pin assignment tables posted on the Microchip website. For SmartFusion2 and IGLOO2 devices, contact Microchip Technical Support for more details. For SSN analysis, see device-specific documentation such as the SSO application note. | 2022.2 | 2023.1 | Fixed |
| PolarFire | Core version of 160 MHz oscillator generates the clock name Workaround: Manually modify the derived constraints clock name to | 2022.3 | 2023.1 | Fixed |
| PolarFire | The maximum clock frequency on the regional clocks (RX_CLK_R/TX_CLK_R on serdes and RX_CLK on lanectrl) in PA5M300XT do not match the frequency on the datasheet. | 12.5 | Open | |
| PolarFire | The violation report shows violations (red cross), but the timing report does not (green check). In this case, there is indeed a timing violation and the red cross is correct. | 12.5 | 2023.1 | Fixed |
| PolarFire | The Power Estimator does not support ES devices and EVAL packages. | 2021.2 | N/A | Will not fix |
| PolarFire SoC | MPFS250 MIL Timing Reports Data State is marked Preliminary instead of Production. | 2022.3 | 2023.1 | Fixed |
12.4 SmartDebug
(Ask a Question)The following table lists the known issues and limitations associated with SmartDebug.
| Family | Description | Version Identified | Version Fixed | Status |
|---|---|---|---|---|
All | If a FlashPro6 programmer is connected to a Linux workstation and you select Refresh/Rescan Programmers, SmartDebug returns the following error message:
If this occurs, SmartDebug displays the following message until you follow the published workaround:
Workaround: Disconnect the programmer and reconnect to PC. | 2023.2 | 2024.2 | Fixed |
All | Exporting component description of HDL+ core causes Libero SoC to crash. | 2022.2 | 2022.3 | Fixed |
PolarFire | Designs using DDR controller with FHB enabled may crash during the compiling stage with the following error message:
| 12.8 | 2022.3 | Fixed |
PolarFire | Using generates the following error message if you try to
access register lane on Quad 4 and Quad 5 for the MPF500 devices:
| 2022.2 | 2022.3 | Fixed |
| PolarFire, PolarFire SoC | PolarFire SoC MSS register access: MSS read error occurs
on the CFG_DDR_SGMII_PHY group of registers with
the following error
message:Currently, there is
no workaround for this issue. | 2021.1 | 2024.2 | Fixed |
| PolarFire SoC | If Dual mode PCIe design is considered in SmartDebug, the PCIe debug feature shows Data Rate, Link Width, and other parameters for PCIe1, but not for PCIe0. | 12.5 | Open |
12.5 SmartHLS™
(Ask a Question)The following table lists the known issues and limitations associated with SmartHLS.
| Family | Description | Version Identified |
Version Fixed |
Status |
|---|---|---|---|---|
| All | In Eclipse, when you add a picture to the existing project by dragging the picture to the project explorer, Eclipse crashes. If you want to add a picture, you can right-click the project and add it by importing from the File System. | 2025.1 | - | Open |
| All | Currently, SmartHLS™ does not support checking Installation History.
Opening this tab displays the following error message:
| 2025.1 | - | Open |
| All | After the project is created, the first time
you right-click to build or clean, the following message appears. This does not impact
functionality.
| 2025.1 | - | Open |
| All | Currently, if you use shls
-g on the Linux command line without having valid licenses, the following
error message appears and you cannot launch
IDE:You
can still compile and run software from the command line using shls
sw_compile and shls sw_run. | 2025.1 | - | Open |
| All | On Ubuntu, Eclipse does not support external browsers installed by Snap. Make
sure your default browser is not installed by Snap, or you can set the external browser from . Select the browser of your choice and click Apply. | 2025.1 | - | Open |
|
All |
In the SmartHLS IDE, you might see red underlines on function calls, with the message that the function could not be resolved, as shown in the following figure: ![]() To fix the red underlines, select . This fixes any Eclipse indexing issues that result in library functions being underlined in red. ![]() For additional information about this known issue and the figures, click here: https://github.com/MicrochipTech/fpga-hls-examples/tree/main/Training1 | 2024.1 | - |
Open |
|
All |
When you use the SmartHLS IDE in the Ubuntu environment, switching tabs while adding source files at the SmartHLS C/C++ project creation stage stops the IDE from responding and requires you to quit the IDE: ![]() To avoid this issue, do not switch tabs while adding source files to the new project being created. | 2024.1 | - |
Open |
|
All |
When
ap_int/ap_uint type is used in the conditional operator ( ?: ), explicit target type casting
is needed in conditional expression that contains primitive operand. For
example:ap_int<12> a, b, c; a = (b > 0)? a : (ap_int<12>)(a+1); c = (b == 2)? (ap_int<12>)0 : (ap_int<12)(a+1); Missing explicit target type casting in the above statements generates the following compiler error message:
| 2024.1 | - |
Open |
|
All |
While C++ template is generally supported in SmartHLS, there are two known scenarios of using templated
top-level functions where SmartHLS may still be able to generate the Verilog code but co-simulation
will fail:
| 2024.1 | - |
Open |
12.6 Programming
(Ask a Question)The following table lists the known issues and limitations associated with Programming and Debug tools.
| Family | Description | Version Found | Version Fixed | Status |
|---|---|---|---|---|
| PolarFire and PolarFire SoC | If the bitstream is configured with the default key (KLK) and Stage 3 SPI flash
binding is set to UEK1 in the Configure Design Initialization Data and Memories
tool, the following error message appears in the log during job file
export:The primary issue occurs when Stage 3 SPI-Flash binding (within the "Configure Design Initialization Data and Memories" tool) is set to UEK1 or UEK2, while the bitstream security (configured via the Configure Security tool) remains set to the default security. In this scenario, no error message is generated, which may result in a RAM initialization failure. Workaround: Manually confirm that Bitstream security configuration (using the Configure Security tool) and SPI-Flash-Binding configuration (under Configure Design Initialization Data and Memories tool) are the same. | 12.0 | 2025.1 | Fixed |
| RT PolarFireSoC | During multiple device programming actions, the log under Security Locks and Configuration Settings displays User Security (DPK1/DPK2) is unlocked instead of User Security (UPK1/UPK2) is unlocked. Workaround: None | 2025.1 | Open | |
| PolarFire and PolarFire SoC | The digest information reported during programming with FP6 acceleration (Turbo) mode does not match the output reported by other programmers or job files generated with the STAPL format. Workaround: Use FlashPro4 or FlashPro5 programmer or generate the FlashPro Express job file using STAPL format. | 2024.2 | 2025.1 | Fixed |
| SmatFusion2/IGLOO2 | Exporting SVF bitstream files from Libero for SmartFusion2/IGLOO2 devices with eNVM sanitization option turned ON will fail when running ERASE action using the *_ERASE.svf file. Workaround: Create eNVM client(s) with all zeros filling the entire eNVM memory space and use *_PROGRAM.svf file to sanitize the eNVM. | 2021.1 | Open | |
| PolarFire SoC | In PolarFire SoC, which uses the One-Way Passcode (OWP) feature, Libero crashes on Linux operating systems if you select Generate HWM from UTC under Advanced Options for *.spi files in the Export Bitstream dialog. | 2022.3 | 2025.1 | Fixed |
| RTG4 | The DSN value reported at the end of the programming action with FP6 acceleration (Turbo) mode is invalid. Workaround: Use FP4 or FP5 programmer or generate the Flash Pro Express job file using STAPL format. | 2024.2 | 2025.1 | Fixed |
| IGLOO2 | For M2S060 devices only, the Erase action might fail after generating a bitstream with the Sanitize ENVM on Erase option enabled. Workaround: Program the device by adding an ENVM client with a size equivalent to the previously programmed ENVM content, filled with all zeros. | 12.6 | 2025.1 | Fixed |
| SmartFusion2 and IGLOO2 | For SmartFusion2 and Igloo2, bitstream generation fails when using eNVM client
with zero’s as content with sizes 126 KB and up with following error
message:Workaround: Create file that
programs zeros in intended pages in one of supported formats (Intel-Hex, Motorola,
etc.,) | 2024.1 | 2025.1 | Fixed |
| SmartFusion2 and IGLOO2 | Exporting SVF bitstream file format fails for devices belonging to SmartFusion2
and IGLOO2 families with following error
message:Workaround:
None. The alternative is to use earlier releases of Libero SoC (v2024.1 or
older). | 2024.2 | 2025.1 | Fixed |
| IGLOO2 and SmartFusion2 | Depending on the design, you might experience an I/O glitch when exiting programming mode, typically following program or verification actions. | 2023.2 | 2024.1 | Fixed |
| RTG4 | Insufficient wait time while exiting programming action runs can cause System Controller to come out of suspend mode in some cases when FlashPro programmer is still connected. Workaround: Disconnect Flashpro programmer and while keeping JTAG TRSTB low, power cycle the board to make sure System Controller remains in suspend mode. | 11.6 | 2024.1 | Fixed |
| All | If Libero SoC or Program & Debug tools are installed on a Linux machine with no sudo access, some configuration files are not copied properly causing the software to crash if programmer access is needed; this includes loading an FPExpress project. Workaround: Install the software in SUDO mode. | 12.0 | 2024.1 | Fixed |
All | Multiple applications cannot access the programming hardware (FlashPro4, FlashPro5, FlashPro6, or eFlashPro6) simultaneously including scanning/refreshing programmers. For example, if Libero is actively running programming actions, do not try to perform any operations in FlashPro Express, including opening a project. The software behavior is unpredictable. Workaround: Use only one application—Libero, FlashPro Express, SmartDebug, Identify, or SoftConsole—at a time. | 12.0 | N/A | Will not fix |
PolarFire SoC | Even though the UI shows the option Keep MSS in operational state during programming for IAP/Auto Update using system services is selected, the generated bitstream does not configure it properly. Therefore, MSS will not be operational during programming. | 2021.1 | 2024.1 | Fixed |
All | During chain programming, Libero crashes if the second device is a different family from the target device when you try to load a PPD file into the second device. Workaround: Use STP files instead of PPD files. | 2022.3 | 2024.1 | Fixed |
All | If Libero SoC is installed in a Linux environment without sudo access, request the admin to install the FlashPro6 libraries after installation. Otherwise, the Libero SoC, FlashPro Express and SmartDebug tools will crash. Workaround: Ask Linux admin to install FlashPro6 libraries by executing ./bin/fp6_env_install. See installation guide for more details. | 2023.2 | N/A | Will not fix |
PolarFire SoC | USB library access issue prevents the support of multiple eFP6 programmers with Libero, FlashPro Express, and SmartDebug. Workaround: Use a single eFlashPro6 programmer per workstation. | 12.6 | Open | |
| PolarFire, PolarFire SoC | If the bitstream is exported in SPI format, the Memory Initialization data stored is always encrypted and binded using the Default KLK regardless of the user-selected binding. | 2023.1 | 2023.2 | Fixed |
PolarFire, PolarFire SoC | Changing security settings doesn’t invalidate generated bitstream in some cases. Running programming action uses a bitstream file generated with previous security settings. Workaround: If using Libero v2023.1 or earlier, re-run generate bitstream regardless of the state of the Generate Bitstream tool. | 2023.1 | 2023.2 | Fixed |
| SmartFusion2, IGLOO2, PolarFire, PolarFire SoCC | FlashPro Express fails to perform any programming action using FlashPro6 using the SPI Slave interface. The JTAG interface is not affected. Workarounds:
| 2021.3 | 2022.2 | Fixed |
All | Libero crashes when you try to switch between programmers using the Select Programmer tool. Workaround:
| 2023.1 | 2023.2 | Fixed |
| SmartFusion2, Igloo2 | BP and Silicon Sculptor 3 programmers error-out with hardware timeout when programming SmartFusion2/IGLOO2 devices using STAPL file. | N/A | 2023.1 | Fixed |
| PolarFire, PolarFire SoC | The following SPI bitstreams for devices cannot be used as SPI bitstream clients in Libero 2022.2 using a Silver and Gold license. Silver license – affected devices:
Gold license – affected devices:
| 2022.2 | 2022.3 | Fixed |
| PolarFire, PolarFire SoC | SPI bitstreams exported prior to Libero v2021.1 cannot be used as SPI bitstream
clients. Libero returns the following error:
| 2022.2 | 2022.3 | Fixed |
| PolarFire, RT PolarFire, PolarFire SoC | Libero shows the incorrect warning/summary message that the SPI Slave interface
is disabled. All SPI pins are disabled when disabling the SPI Slave interface in the
Update Policy in the Configure Security tool. The second statement is incorrect, the
SPI pins are not disabled . | 2022.1 | 2022.3 | Fixed |
| PolarFire, RT PolarFire, PolarFire SoC | Protected components in the custom security are exported in the SPI bit stream. | 2022.2 | 2022.3 | Fixed |
| SmartFusion2, IGLOO2 | If Programming Recovery is enabled in the Configure Programming options tool and is using custom security in Configure Security tool, the DAT bitstream file generated will be incorrect and will not erase the security completely on the device when running ERASE action. | 11.9 | 2022.3 | Fixed |
| PolarFire, PolarFire SoC | If setting permanently write protect fabric in the Configure Permanent Locks tool, the exported bitstream file/job will also program sNVM update protection to be locked for update (i.e., protected by Flashlock/UPK1), even though sNVM updates were allowed without Flashlock/UPK1 in Configure Security tool. | 12.4 | 2022.2 | Fixed |
| PolarFire, PolarFire SoC | If Authenticate action is disabled in the Update Policy of Configure Security tool, the ENC_DATA_AUTHENTICATION action will fail in Libero and FlashPro Express, even when Flashlock/UPK1 is included in the bitstream file. If external zeroization through JTAG/SPI Target is disabled in the JTAG/SPI Target Commands Policy of Configure Security tool, ZEROIZE_LIKE_NEW and ZEROIZE_UNRECOVERABLE actions fail in Libero and FlashPro Express, even when Flashlock/UPK1 is included in the bitstream file. | 12.0 | 2022.2 | Fixed |
PolarFire SoC | For PolarFire SoC Libero designs that contain eNVM, running VERIFY_DIGEST after programming the device will fail with the message eNVM digest verification: FAIL. Workaround : Deselect the procedure DO_ENABLE_ENVM in the VERIFY_DIGEST action | 12.9 | 2022.2 | Fixed |
| PolarFire, PolarFire SoC | Non-recoverable zeroization mode is not programmed with Libero design, which does not have any POR digest configured and no custom security. | 2021.3 | 2021.3 | Fixed |
PolarFire, PolarFire SoC | In Libero designs containing SPI bitstream clients (IAP, Auto Update, or Recovery/Golden) along with a STAGE3 initialization client in the SPI Flash tab of the Configure Design Initialization Data and Memories tool, the output of the Export SPI Flash Image tool does not contain data for the STAGE3 initialization clients. Workaround: If possible, use the Generate SPI Flash Image and program in Libero or Export FlashPro Express job with SPI Flash and program via FlashPro Express. | 2021.2 | 2022.2 | Fixed |
| All | Performing READ_SPI_IMAGE using large-density flash devices is not recommended and can cause Flash Pro Express to become unresponsive. | 2022.3 | Open | |
| All | Programming actions with FlashPro6 will fail when connected to Windows 10 computers with 11th-generation Intel core processors. Workaround: Use FlashPro5 programmers. | 2021.1 | Open | |
| All | When performing any action with FlashPro6, the following error message could
appear:Workaround:
This error could be caused by the programmer being out of sync with the software
application. To resolve this issue, unplug the USB cable from either the programmer
or the host PC, and then reconnect it to reset the programmer. | 2021.2 | N/A | Will not fix |
| PolarFire | If you want to reprogram the Fabric/sNVM with UEK1/UEK2 bitstreams, and the program action is disabled in update policy, manually enable the plaintext pass keys when exporting the UEK1/UEK2 bitstreams. Currently, this option is unselected by default. | 2022.3 | 2023.1 | Fixed |
| PolarFire SoC | The plaintext pass keys are included in the bitstream even in the cases where
protected components are not selected. The following two conditions apply:
Manually enable exporting the plaintext pass keys in the export bitstream tool if the Fabric/sNVM and eNVM are open for updates and the Program action is disabled in the Update Policy. Otherwise, you will not be able to run the Program action with UEK1/UEK2. | 2022.3 | 2023.1 | Fixed |
| PolarFire, PolarFire SoC | Using SPI-Slave method with FlashPro6, verify digest action performs a check on all available components rather than the selected ones. | 2022.3 | Open | |
| PolarFire SoC | Some test cases fail with the following error message:Workaround: Power cycle the Icicle board and rescan the programmers. | 12.6 | Open | |
| PolarFire SoC | If an Icicle kit is connected to one or more USB hubs, you may receive the following error message: | 2021.1 | Open | |
| SmartFusion, RTG4, PolarFire, PolarFire SoC | You might see the following error message during
programming:This is most likely a USB connection issue. This error also appears if the connection is interrupted. The error message may be different, depending on where the packet is dropped during verify. However, the error code will always be set to 4, which indicates a general device I/O error. | 12.6 | N/A | Will not Fix |
| SmartFusion2, IGLOO2 | FlashLock/UPK1 cannot be used to allow debug access through JTAG (1149.1) if it is disabled in the Debug Policy in Configure Security tool. | 2022.1 | 2023.1 | Fixed |
| SmartFusion2, IGLOO2 | If all the keys (UEK1/UEK2/UEK3) are disabled in keymode policy, ERASE and VERIFY actions fail with the following error message:Workaround: Do not run ERASE and VERIFY actions when all the keys (UEK1/UEK2/UEK3) are disabled in keymode policy. | 2021.3 | Open |
12.7 Installation and System Limitations
(Ask a Question)The following table lists the known installation and system issues and limitations.
| Description | Version Found | Version Fixed | Status |
|---|---|---|---|
All standalone installations are included as part of the Libero SoC Design Suite. Due to system limitations, each standalone tool appears as Libero SoC in the Windows Add/Remove Programs menu. Workaround: None | 2025.1 | Open | |
When running the Libero 2024.2 installer in Windows 10 or 11, you might encounter the following error message:
Workaround: Perform the following procedure:
| 2024.2 | 2025.1 | Fixed |
Customers using a Libero node locked license might encounter the following error message:
Workaround:
| 2024.1 | 2024.1 | Fixed |
The stand-alone Program and Debug Linux installer (v2022.2) does not install FlashPro 6 libusb libraries automatically. Workaround: Execute fp6_env_install located in ./Program_Debug_Tool/bin/ | 2022.2 | 2022.3 | Fixed |
The Libero SoC online help reports JavaScript errors when you click microchip.com links. Workaround: The default browser for help files is Internet Explorer. To avoid this issue, copy the desired link and open it in a supported browser, such as Chrome, Firefox, or Edge. | 2022.2 | Open | |
The following link provides information about FlexNet error codes: https://knowledge.autodesk.com/search-result/caas/sfdcarticles/sfdcarticles/Common-FlexNet-error-codes.html. | N/A | N/A | N/A |
If the installer does not boot in graphical mode, additional X window system libraries might be required. For RHEL/CentOS, the following system package is recommended: $ sudo yum install -y libXau libX11 libXi libxcb libXext libXtst libXrender | N/A | N/A | N/A |
Many antivirus and Host-based Intrusion Prevention System (HIPS) tools flag executable and prevent them from running. To avoid this problem, modify your security setting by adding exceptions for specific executable. This is configured in the antivirus tool. Contact the tool provider for assistance. Many users run Libero SoC PolarFire successfully with no modification to their antivirus software. Microchip is aware of issues for some antivirus tool settings that occur when using Symantec®, McAfee®, Avira™, Sophos®, and Avast™ tools. The combination of operating system, antivirus tool version, and security settings all contribute to the end result. Depending on the environment, the operation of Libero SoC, ModelSim ME, and/or Synplify Pro ME may or may not be affected. All public releases of Libero software are tested with several antivirus tools before they are released to ensure that they are not infected. In addition, the Microchip software development and testing environment is also protected by antivirus tools and other security measures. | N/A | N/A | N/A |