CxFIFOSTA1

CAN FIFO Status Register 1
Note:
  1. The individual bytes in this multibyte register can be accessed with the following register names:
    • CxFIFOSTAyT: Accesses the top byte FIFOSTAy[31:24]
    • CxFIFOSTAyU: Accesses the upper byte FIFOSTAy[23:16]
    • CxFIFOSTAyH: Accesses the high byte FIFOSTAy[15:8]
    • CxFIFOSTAyL: Accesses the low byte FIFOSTAy[7:0]
  2. [y] denotes FIFO number, from 1 to 3.
  3. FIFOCI[4:0] gives a zero-indexed value to the message in the FIFO. If the FIFO is four message deep (FSIZE = 3), FIFOCIx will take on a value of 0 to 3, depending on the state of the FIFO.
  4. This bit is updated when a message completes (or aborts) or when the FIFO is reset.
  5. This bit is reset on any read of this register or when the TXQ is reset.
Name: CxFIFOSTA1
Address: 0x0160

Bit 3130292827262524 
          
Access  
Reset  
Bit 2322212019181716 
          
Access  
Reset  
Bit 15141312111098 
    FIFOCI[4:0] 
Access [R[R[R[R[R 
Reset 00000 
Bit 76543210 
 TXABTTXLARBTXERRTXATIFRXOVIFTFERFFIFTFHRFHIFTFNRFNIF 
Access RRRHS/CHS/CRRR 
Reset 00000000 

Bits 12:8 – FIFOCI[4:0]  FIFO Message Index

NameDescription
TXEN = 1(FIFO configured as a transmit buffer) A read of this register will return an index to the message that the FIFO will next attempt to transmit
TXEN = 0(FIFO configured as a receive buffer) A read of this register will return an index to the message that the FIFO will use to save the next message

Bit 7 – TXABT  Message Aborted Status

ValueDescription
1 Message was aborted
0 Message completed successfully

Bit 6 – TXLARB  Message Lost Arbitration Status

ValueDescription
1 Message lost arbitration while being sent
0 Message did not lose arbitration while being sent

Bit 5 – TXERR  Error Detected During Transmission

ValueDescription
1 A bus error occurred while the message was being sent
0 A bus error did not occur while the message was being sent

Bit 4 – TXATIF Transmit Attempts Exhausted Interrupt Pending

ValueNameDescription
1 TXEN = 1(FIFO configured as a transmit buffer) Interrupt is pending
0 TXEN = 1(FIFO configured as a transmit buffer) Interrupt is not pending
x TXEN = 0(FIFO configured as a receive buffer) Unused, reads as ‘0’

Bit 3 – RXOVIF Receive FIFO Overflow Interrupt Flag

ValueNameDescription
x TXEN = 1(FIFO configured as a transmit buffer) Unused, reads as ‘0’
1 TXEN = 0(FIFO configured as a receive buffer) Overflow event has occurred
0 TXEN = 0(FIFO configured as a receive buffer) No overflow event occurred

Bit 2 – TFERFFIF Transmit/Receive FIFO Empty/Full Interrupt Flag

ValueNameDescription
1 TXEN = 1(FIFO configured as a transmit buffer) FIFO is empty
0 TXEN = 1(FIFO configured as a transmit buffer) FIFO is not empty, at least one message is queued to be transmitted
1 TXEN = 0(FIFO configured as a receive buffer) FIFO is full
0 TXEN = 0(FIFO configured as a receive buffer) FIFO is not full

Bit 1 – TFHRFHIF Transmit/Receive FIFO Half Empty/Half Full Interrupt Flag

ValueNameDescription
1 TXEN = 1(FIFO configured as a transmit buffer) FIFO is less than or equal to half full
0 TXEN = 1(FIFO configured as a transmit buffer) FIFO is greater than half full
1 TXEN = 0(FIFO configured as a receive buffer) FIFO is greater than or equal to half full
0 TXEN = 0(FIFO configured as a receive buffer) FIFO is less than half full

Bit 0 – TFNRFNIF Transmit/Receive FIFO Not Full/Not Empty Interrupt Flag

ValueNameDescription
1 TXEN = 1(FIFO configured as a transmit buffer) FIFO is not full
0 TXEN = 1(FIFO configured as a transmit buffer) FIFO is full
1 TXEN = 0(FIFO configured as a receive buffer) FIFO is not empty, has at least one message
0 TXEN = 0(FIFO configured as a receive buffer) FIFO is empty
The individual bytes in this multibyte register can be accessed with the following register names: CxFIFOSTAyT: Accesses the top byte FIFOSTAy[31:24] CxFIFOSTAyU: Accesses the upper byte FIFOSTAy[23:16] CxFIFOSTAyH: Accesses the high byte FIFOSTAy[15:8] CxFIFOSTAyL: Accesses the low byte FIFOSTAy[7:0] [y] denotes FIFO number, from 1 to 3. FIFOCI[4:0] gives a zero-indexed value to the message in the FIFO. If the FIFO is four message deep (FSIZE = 3), FIFOCIx will take on a value of 0 to 3, depending on the state of the FIFO. This bit is updated when a message completes (or aborts) or when the FIFO is reset. This bit is reset on any read of this register or when the TXQ is reset.