Calculates the signed integer exponent of a double precision floating-point value.
Include
<math.h>
Prototype
int ilogbl(long double x);
Argument
x
Return Value
Returns the exponent of x
as a signed integer value. If
x
is 0, it returns the value FP_ILOGB0
; if
x
is infinite, it returns the value INT_MAX
; if
x
is a NaN it returns the value FP_ILOGBNAN
;
otherwise, this will yield the same value as the corresponding logb
function cast to type int
. A range error may occur if
x
is 0.
Remarks
A range error might occur if x
is 0.
Example
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x;
int y;
errno = 0;
x = 13.45;
y = ilogbl(x);
if (errno)
perror("Error");
printf("The exponent of %f is %d\n", x, y);
errno = 0;
x = 0.0;
y = ilogbl(x);
if (errno)
perror("Error");
printf("The exponent of %f is %d\n", x, y);
errno = 0;
x = -2.0;
y = ilogbl(x);
if (errno)
perror("Error");
printf("The exponent of %f is %d\n", x, y);
}
Example Output
The exponent of 13.450000 is 3
The exponent of 0.000000 is -2147483648
The exponent of -2.000000 is 1