Calculates the base-2 logarithm of a double precision floating-point value.
Include
<math.h>
Prototype
double log2(double x);
Argument
x
Return Value
Returns the base-2 logarithm of x
. -inf
is
returned if x
is 0 and NaN is returned if x
is a
negative number.
Remarks
A domain error occurs for argument less than 0. A range error might occur if the argument is equal to zero.
Example
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x, y;
errno = 0;
x = 2.0;
y = log2(x);
if(errno)
perror("Error");
printf("The base-2 logarithm of %f is %f\n", x, y);
errno = 0;
x = 0.0;
y = log2(x);
if(errno)
perror("Error");
printf("The base-2 logarithm of %f is %f\n", x, y);
errno = 0;
x = -2.0;
y = log2(x);
if(errno)
perror("Error");
printf("The base-2 logarithm of %f is %f\n", x, y);
}
Example Output
The base-2 logarithm of 2.000000 is 1.000000
The base-2 logarithm of 0.000000 is -inf
Error: domain error
The base-2 logarithm of -2.000000 is nan