The compiler supports the use of type qualifiers on structures. When a
qualifier is applied to a structure, all of its members will inherit this qualification. In
the following example the structure is qualified const
.
const struct {
int number;
int *ptr;
} record = { 0x55, &i }; // record place in program memory
In this case, the entire structure will be placed into the program space
and each member will be read-only. Remember that all members are usually initialized if a
structure is const
as they cannot be initialized at runtime.
If the members of the structure were individually qualified
const
, but the structure was not, then the structure would be
positioned into RAM, but each member would be read-only. Compare the following structure
with the above.
struct {
const int number;
int * const ptr;
} record = { 0x55, &i }; // record placed in data memory