A macro that writes the timer peripheral.
Include
<xc.h>
Prototype
void WRITETIMERx(int n);
Remarks
The WRITETIMERx()
macro is available for PIC18
projects and writes the 2-byte argument to both bytes of the TMRx register, where
x is one of the digits 0, 1 or 3. It ensures that the registers are written
in the correct order, which cannot be guaranteed when accessing the entire TMR SFR
directly.
Example
#include <xc.h>
int main(void)
{
WRITETIMER0(0x4A);
}