Performs a binary search.
Include
<stdlib.h>
Prototype
void *bsearch(const void *key, const void *base,
size_t nelem, size_t size, int (*cmp)(const void *ck,
const void *ce));
Arguments
key
base
nelem
size
cmp
Arguments to the comparison function are as follows.
ck
ce
Return Value
Returns a pointer to the object being searched for if found; otherwise,
returns NULL
.
Remarks
The value returned by the compare function is <0 if ck
is less than ce
, 0 if ck
is equal to
ce
or >0 if ck
is greater than
ce
.
In the following example, qsort
is used to sort the list before
bsearch
is called. bsearch
requires the list to be
sorted according to the comparison function. This comp
uses ascending
order.
Example
#include <stdlib.h>
#include <stdio.h>
#define NUM 7
int comp(const void *e1, const void *e2);
int main(void)
{
int list[NUM] = {35, 47, 63, 25, 93, 16, 52};
int x, y;
int *r;
qsort(list, NUM, sizeof(int), comp);
printf("Sorted List: ");
for (x = 0; x < NUM; x++)
printf("%d ", list[x]);
y = 25;
r = bsearch(&y, list, NUM, sizeof(int), comp);
if (r)
printf("\nThe value %d was found\n", y);
else
printf("\nThe value %d was not found\n", y);
y = 75;
r = bsearch(&y, list, NUM, sizeof(int), comp);
if (r)
printf("\nThe value %d was found\n", y);
else
printf("\nThe value %d was not found\n", y);
}
int comp(const void *e1, const void *e2)
{
const int * a1 = e1;
const int * a2 = e2;
if (*a1 < *a2)
return -1;
else if (*a1 == *a2)
return 0;
else
return 1;
}
Example Output
Sorted List: 16 25 35 47 52 63 93
The value 25 was found
The value 75 was not found