Baseline devices can use the OPTION and TRIS SFRs, which are not memory mapped.
The definition of these registers use a special qualifier,
__control
, to indicate that the registers are write-only, outside
the normal address space and must be accessed using special instructions.
When these SFRs are written in C code, the compiler will use the appropriate instruction to store the value. For example, to set the TRIS register, the following code:
TRIS = 0xFF;
would be encoded by the compiler as:
movlw 0ffh
TRIS
Those Baseline PIC devices which have more than
one output port can have __control
definitions for objects:
TRISA
, TRISB
and TRISC
, which
are used in the same manner as described above.
Any register that uses the __control
qualifier must be
accessed as a full byte. If you need to access bits within the register, copy the
register to a temporary variable first, then access that temporary variable as
required.