The assembly generated from C source code by the compiler will use certain registers in the PIC MCU register set. Most importantly, the compiler assumes that nothing other than code it generates can alter the contents of these registers.
The registers that are special and which are used by the compiler are listed in the following table.
Register name | Applicable devices |
---|---|
W |
All 8-bit devices |
STATUS |
All 8-bit devices |
PCLATH |
All Mid-range devices |
PCLATH ,
PCLATU |
All PIC18 devices |
BSR |
Enhanced Mid-range and PIC18 devices |
FSR |
Non-Enhanced Mid-range devices |
FSR0L ,
FSR0H , FSR1L ,
FSR1H |
Enhanced Mid-range and PIC18 devices |
FSR2L ,
FSR2H |
All PIC18 devices |
TBLPTRL ,
TBLPTRH , TBLPTRU ,
TABLAT |
All PIC18 devices |
PRODL ,
PRODH |
All PIC18 devices |
btemp ,
wtemp , ttemp , ltemp ,
lltemp |
Enhanced Mid-range and PIC18 devices |
The xtemp
registers are variables that the
compiler treats as registers. These are saved like any other register if they are used in
interrupt code. The lltemp
register is only available when using Enhanced
Mid-range or PIC18 devices.
The compiler will not be aware of changes to a register’s value when the
register itself is a C lvalue (assignment destination). For example, if the statement
WREG = 0;
was encoded using the clrf
instruction, the
compiler would not consider this as modifying the W register. Nor should these registers be
changed directly by in-line assembly code, as shown in the following example which modifies
the ZERO bit in the STATUS register.
#include <xc.h>
void getInput(void)
{
asm("bcf ZERO"); //do not write using inline assembly code
process(c);
}
If any of the applicable registers listed in the table are used by interrupt code, they will be saved and restored when an interrupt occurs, either in hardware or software (see Context Switching).