Ends the use of ap
.
Include
<stdarg.h>
Prototype
#define va_end(va_list ap)
Argument
ap |
pointer to list of arguments |
Remarks
After a call to va_end
, the argument list pointer,
ap
, is considered to be invalid. Further calls to
va_arg
should not be made until the next va_start
.
In the 16-bit compiler, va_end
does nothing, so this call is not
necessary but should be used for readability and portability.
Example
See va_arg
.