Identifiers are used to represent C objects and functions and must conform to strict rules.
A C identifier is a sequence of letters and digits where the underscore
character “_
” counts as a letter. Identifiers cannot start with a digit.
Although they can start with an underscore, such identifiers are reserved for the
compiler’s use and should not be defined by C source code in your programs. Such is not the
case for assembly-domain identifiers.
Identifiers are case sensitive, so main
is different to
Main
.
Up to 255 characters are significant in an identifier. If two identifiers differ only after the maximum number of significant characters, then the compiler will consider them to be the same symbol.