The format of integral constants specifies their radix. MPLAB XC8 supports the standard radix specifiers, as well as ones which enables binary constants to be specified in C code.
The formats used to specify the radices are tabulated below. The letters used to specify binary or hexadecimal radices are case insensitive, as are the letters used to specify the hexadecimal digits.
Radix | Format | Example |
---|---|---|
binary | 0bnumber or
0Bnumber |
0b10011010 |
octal | 0number |
0763 |
decimal | number |
129 |
hexadecimal | 0xnumber or
0Xnumber |
0x2F |
Any integral constant will have a type of int
,
long int
or long long int
, so that the type can hold
the value without overflow. Constants specified in octal or hexadecimal can also be
assigned a type of unsigned int
, unsigned long int
or
unsigned long long int
if their signed counterparts are too small to
hold the value.
The default types of constants can be changed by the addition of a suffix
after the digits; e.g., 23U
, where U
is the suffix. The
table below shows the possible combination of suffixes and the types that are considered
when assigning a type. For example, if the suffix l
is specified and the
value is a decimal constant, the compiler will assign the type long int
,
if that type will hold the constant; otherwise, it will assigned long long
int
. If the constant was specified as an octal or hexadecimal constant, then
unsigned types are also considered.
Suffix | Decimal | Octal or Hexadecimal |
---|---|---|
u or
U |
unsigned int
|
unsigned int
|
l or
L |
long int
|
long int
|
u or U , and
\ or L |
unsigned long int
|
unsigned long int
|
ll or
LL |
long long int |
long long int
|
u or U , and
ll or LL |
unsigned long long
int |
unsigned long long
int |
Here is an example of code that can fail because the default type assigned to a constant is not appropriate:
unsigned long int result;
unsigned char shifter;
shifter = 20;
result = 1 << shifter; // oops!
The constant 1 (one) will be assigned an
int
type. If the size of an int type on the compiler being used is
hence the value 1 shifted left 20 bits will yield the result 0, not 0x100000.
The following uses a suffix to change the type of the constant, hence ensure the shift result has an unsigned long type.
result = 1UL << shifter;