Classifies its argument as one of several floating-point categories.
Include
<math.h>
Prototype
int isgreater(floating-point x);
Argument
x
Return Value
Classifies its argument as one of several floating-point categories, such as
FP_NAN
, FP_ZERO
etc.
Example
#include <math.h>
#include <stdio.h>
int main(void)
{
double x;
int b;
x = 0.0;
b = fpclassify(x);
if(b == FP_ZERO)
printf("The value %f has been classified as a floating-point zero\n", x);
}
Example Output
The value 0.000000 has been classified as a floating-point zero