At the bottom of each assembly list file is a symbol table. This differs
from the symbol table presented in the map file (see Symbol Table) in two ways:
Only symbols associated with the assembly module, from which the list
file is produced (as opposed to the entire program) are listed.
Local as well as global symbols associated with that module are
listed.
Each symbol is listed along with the address it has been assigned.