This flag is deprecated. Consider, instead, using the
optim
psect flag.
The inline
psect flag is used by the code generator to
tell the assembler that the contents of a psect can be inlined. If this operation is
performed, the contents of the inline
psect will be copied and used to
replace calls to the function defined in the psect.