Prints formatted text to stdout
.
Include
<stdio.h>
Prototype
int printf(const char *format, ...);
Arguments
format
...
Return Value
Returns number of characters generated or a negative number if an error occurs.
Remarks
This function relies on the
putch
function to determine the destination of the standard output
stream. A putch
function must be written for each project that uses
printf
, and the project must include code that initializes any
peripherals used by this routine. A stub for putch
can be found in the
sources directory of the compiler. Ensure the source code for your
putch
added to your project once it is complete. An example
putch
function that prints to a USART might be similar to:
void putch(char data)
{
while( ! TXIF)
continue;
TXREG = data;
}
There must be exactly the same number of arguments as there are format specifiers. If the are less arguments than match the format specifiers, the output is undefined. If there are more arguments than match the format specifiers, the remaining arguments are discarded. Each format specifier begins with a percent sign followed by optional fields and a required type as shown here:
%[flags][width][.precision][size]type
flags
- |
Left justify the value within a given field width. |
0 |
Use 0 for the pad character instead of space (which is the default). |
+ |
Generate a plus sign for positive signed values. |
space | Generate a space or signed values that have neither a plus nor a minus sign. |
# |
To prefix 0 on an octal conversion, to prefix 0x or 0X on a hexadecimal conversion, or to generate a decimal point and fraction digits that are otherwise suppressed on a floating-point conversion. |
width
Specify the number of characters to generate for the conversion. If the asterisk (*) is used instead of a decimal number, the next argument (which must be of type int) will be used for the field width. If the result is less than the field width, pad characters will be used on the left to fill the field. If the result is greater than the field width, the field is expanded to accommodate the value without padding.
precision
The field width can be followed with dot (.
) and a decimal integer
representing the precision that specifies one of the following:
If the period appears without the integer, the integer is assumed to be zero. If the asterisk (*) is used instead of a decimal number, the next argument (which must be of type int) will be used for the precision.
size
h modifier | Used with type d, i, o, u, x, X;
converts the value to a short int or unsigned
short int . |
h modifier | Used with n; specifies that the
pointer points to a short int . |
l modifier | Used with type d, i, o, u, x, X;
converts the value to a long int or unsigned
long int . |
l modifier | Used with n; specifies that the
pointer points to a long int . |
l modifier | Used with c; specifies a wide character. |
l modifier | Used with type e, E, f, F, g, G;
converts the value to a double . |
ll modifier | Used with type d, i, o, u, x, X;
converts the value to a long long int or
unsigned long long int . |
ll modifier | Used with n; specifies that the
pointer points to a long long int . |
L modifier | Used with e, E, f, g, G; converts
the value to a long double . |
type
d, i | signed
int . |
o | unsigned int in
octal. |
u | unsigned int in
decimal. |
x | unsigned int in
lowercase hexadecimal. |
X | unsigned int in
uppercase hexadecimal. |
e, E | double in
scientific notation. |
f | double decimal
notation. |
g, G | double (takes the
form of e, E or f as appropriate). |
c | char - a single
character. |
s | string . |
p | value of a pointer. |
n | The associated argument shall be an integer pointer into which is placed the number of characters written so far. No characters are printed. |
% | A % character is
printed. |
Example
#include <stdio.h>
int main(void)
{
/* print a character right justified in a 3 */
/* character space. */
printf("%3c\n", 'a');
/* print an integer, left justified (as */
/* specified by the minus sign in the format */
/* string) in a 4 character space. Print a */
/* second integer that is right justified in */
/* a 4 character space using the pipe (|) as */
/* a separator between the integers. */
printf("%-4d|%4d\n", -4, 4);
/* print a number converted to octal in 4 */
/* digits. */
printf("%.4o\n", 10);
/* print a number converted to hexadecimal */
/* format with a 0x prefix. */
printf("%#x\n", 28);
/* print a float in scientific notation */
printf("%E\n", 1.1e20);
/* print a float with 2 fraction digits */
printf("%.2f\n", -3.346);
/* print a long float with %E, %e, or %f */
/* whichever is the shortest version */
printf("%Lg\n", .02L);
}
Example Output
a
-4 | 4
0012
0x1c
1.100000E+20
-3.35
0.02