Returns the argument rounded to the nearest integer value.
Include
<math.h>
Prototype
long long int llrintf(float x);
Argument
x
Return Value
Returns the value of x
rounded to the nearest integer value
using the current rounding direction. The rounded integer is returned as an integer
value.
Remarks
The value returned is unspecified if the rounded value is outside the range
of the return type. A range error may occur if the magnitude of x
is
too large.
Example
#include <math.h>
#include <stdio.h>
int main(void)
{
float x;
long long int y;
x = 10.103;
y = llrintf(x);
printf("The nearest integer value to %f is %lld\n", x, y);
x = 10.51;
y = llrintf(x);
printf("The nearest integer value to %f is %lld\n", x, y);
}
Example Output
The nearest integer value to 10.103000 is 10
The nearest integer value to 10.510000 is 11