The functions, variables, types, and preprocessor macros defined by the standard compiler library are summarized in this chapter, listed under the header file which declares them.
Note that where use of the
printf()
function is made in example code, this assumes that the
putch()
function has been defined to suit the peripheral representing
the stdout
stream. Initialization of that peripheral must also be
performed before you attempt to print.