Test for a printable character (includes a space).
Include
<ctype.h>
Prototype
int isprint (int c);
Argument
c
Return Value
Returns a non-zero integer value if the character, c
, is
printable; otherwise, returns zero.
Remarks
A character is considered to be a printable character if it is in the range 0x20 to 0x7e inclusive.
Example
#include <ctype.h>
#include <stdio.h>
int main(void)
{
int ch;
ch = '&';
if (isprint(ch))
printf("& is a printable character\n");
else
printf("& is NOT a printable character\n");
ch = '\t';
if (isprint(ch))
printf("a tab is a printable character\n");
else
printf("a tab is NOT a printable character\n");
}
Example Output
& is a printable character
a tab is NOT a printable character