Assembly language can be mixed with C code using two different
techniques:
- Assembly code placed in separate
assembly source modules.
- Assembly code placed inline with C
code.
Note: The more assembly code a project contains, the more
difficult and time consuming will be its maintenance. Assembly code might need revision if
the compiler is updated due to differences in the way the updated compiler may work. These
factors do not affect code written in C.
If assembly must be added, it is preferable to
write this as a self-contained routine in a separate assembly module, rather than in-lining
it in C code.