A builtin function that delays execution for the specified time.
Include
<xc.h>
Prototype
void __delay_us(unsigned long time);
Argument
time
Remarks
This is an inbuilt function that is expanded by the code generator. When called, this routine expands to an in-line assembly delay sequence. The sequence will consist of code that delays for the number of micro seconds specified as the argument. The argument must be a constant expression.
This macro require the prior definition of the preprocessor macro
_XTAL_FREQ
, which indicates the system frequency. This macro should
equate to the oscillator frequency (in hertz) used by the system. Note that this macro
only controls the behavior of these delays and does not affect the device execution
speed.
The __delay_us()
builtin function can use loops and the
nop
instruction to implement the delay.
An error will result if the requested delay is not a constant expression or is too large. For larger delays, call this function multiple times.
Example
#include <xc.h>
int main (void)
{
__delay_us(10); // delay for 10 micro seconds
}