Put a character to stdout
.
Include
<stdio.h>
Prototype
int putchar(int c);
Argument
c
Return Value
Returns the character or EOF
if an error occurs or end-of-file is
reached.
Remarks
Same effect as fputc
with stdout
as an argument.
Example
#include <stdio.h>
int main(void)
{
char *y;
char buf[] = "This is text\n";
int x;
x = 0;
for (y = buf; (x != EOF) && (*y != '\0'); y++)
x = putchar(*y);
}
Example Output
This is text