Any const
-qualified object which has static storage
duration and which has file scope can be placed at an absolute address in program
memory.
For example:
const int settings[] __at(0x200) = { 1, 5, 10, 50, 100 };
will place the array settings
at address 0x200 in the
program memory.
Note that the __at()
construct can be placed before or after the variable identifier in the definition, but to
be compatible with the C90 standard, it should be place after the identifier.
An uninitialized
extern const
object can be made absolute and is useful when you want to
define a placeholder object that does not make a contribution to the output file.