Puts a character to the stream.
Include
<stdio.h>
Prototype
int putc(int c, FILE *stream);
Arguments
c
stream
FILE
structureReturn Value
Returns the character or EOF
if an error occurs or end-of-file is
reached.
Remarks
putc
is the same as the function fputc
.
Example
#include <stdio.h>
int main(void)
{
char *y;
char buf[] = "This is text\n";
int x;
x = 0;
for (y = buf; (x != EOF) && (*y != '\0'); y++)
{
x = putc(*y, stdout);
putc('|', stdout);
}
}
Example Output
T|h|i|s| |i|s| |t|e|x|t|
|