Rounds the argument rounded to an integer value no large than the argument value.
Include
<math.h>
Prototype
long double truncl(long double x);
Argument
x
Return Value
Returns the value of x
rounded to the nearest integer value
that is no larger in magnitude that the original argument. The rounded integer is
returned as a floating-point value.
Example
#include <math.h>
#include <stdio.h>
int main(void)
{
long double x, y;
x = -10.103;
y = truncl(x);
printf("The nearest integer value to %Lf is %Lf\n", x, y);
x = 10.9;
y = truncl(x);
printf("The nearest integer value to %Lf is %Lf\n", x, y);
}
Example Output
The nearest integer value to -10.103000 is -10.000000
The nearest integer value to 10.900000 is 10.000000