Put a character to stdout
.
Include
<stdio.h>
Prototype
void putch(char c);
Argument
Remarks
The putch()
function is provided as an empty stub which can
be completed as required by the project. It must be defined if you intend to use the
printf()
function. Typically this function will send its argument
to a peripheral that you intend to associate with stdout
.
Example
#include <stdio.h>
const char * x = "This is a string";
int main(void)
{
const char * cp;
cp = x;
while(*cp)
putch(*cp++);
putch(’\n’);
}
Example Output
This is a string