A macro that reads data from the EEPROM memory space.
Include
<xc.h>
Prototype
unsigned char EEPROM_READ(scalar address);
Argument
address
Remarks
This macro is available for all Mid-range devices that implement EEPROM. It is recommended that for PIC18 devices you use MPLAB MCC to generate EEPROM access code, if possible.
Unlike the eeprom_read
function, this macro does not wait
for any concurrent writes to EEPROM to conclude before performing the required
operation. It read the EEPROM and returns the value at the nominated
address
.
Example
#include <xc.h>
#include <stdio.h>
int main (void)
{
unsigned char SerNo;
unsigned char addr = 0x20;
// wait for end-of-write before EEPROM_READ
while(WR)
continue; // read from EEPROM at address
serNo = EEPROM_READ(addr);
printf("The data at EEPROM address %u is %u\n", addr, SerNo);
}