Description
Convert string to unsigned long long
integer value.
Include
<stdlib.h>
Prototype
unsigned long long int strtoull( const char * restrict nptr,
char ** restrict endptr, int base);
Arguments
nptr
endptr
base
Return Value
The converted value, or 0 if the conversion could not be performed.
Remarks
The strtoull
function attempts to convert the first part
of the string pointed to by nptr
to a unsinged long
long
integer value.
Any initial whitespace characters in the string are
skipped. The following characters representing the integer are assumed to be in a
radix specified by the base
argument. Conversion stops once an
unrecognized character is encountered in the string. If the correct converted value
is out of range, the value of the macro ERANGE
is stored in
errno
.
If the value of base
is zero, the characters
representing the integer can be in any valid C constant form (i.e., in decimal,
octal, or hexadecimal), but any integer suffix is ignored. If the value of base is
between 2 and 36 (inclusive), the expected form of the integer characters is a
sequence of letters and digits representing an integer with the radix specified by
base
, optionally preceded by a plus or minus sign, but again,
the integer suffix is ignored. The letters from a
(or
A
) through z
(or Z
) are
ascribed the values 10 through 35; only letters and digits whose ascribed values are
less than that of base
are permitted. If the value of
base
is 16, the characters 0x
or
0X
may optionally precede the sequence of letters and digits,
following the sign if present.
Example
#include <stdlib.h> /* for strtoull */
#include <stdio.h> /* for printf */
int main(void)
{
char * string = "-1234abcd";
char * final;
unsigned long long result;
result = strtoull(string, &final, 10);
printf("The integer conversion of the string \"%s\" is %llu; final string part is \"%s\"\n", string, result, final);
}
Example Output
The integer conversion of the string "-1234abcd" is 18446744073709550382; final string part is "abcd"