Calculates the trigonometric arc cosine function of a double precision floating-point value.
Include
<math.h>
Prototype
double acos (double x);
Argument
x
Return Value
Returns the arc cosine in radians in the range of 0 to pi (inclusive).
Remarks
A domain error occurs if x is less than -1 or greater than 1.
Example
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x,y;
errno = 0;
x = -2.0;
y = acos (x);
if (errno)
perror("Error");
printf("The arccosine of %f is %f\n", x, y);
errno = 0;
x = 0.10;
y = acos (x);
if (errno)
perror("Error");
printf("The arccosine of %f is %f\n", x, y);
}
Example Output
Error: domain error
The arccosine of -2.000000 is nan
The arccosine of 0.100000 is 1.470629