Search for the last occurrence of a specified character in a string.
Include
<string.h>
Prototype
char *strrchr(const char *s, int c);
Arguments
s
c
Return Value
Returns a pointer to the location of the match if successful; otherwise, returns a null pointer.
Remarks
This function searches the string s
to find the last
occurrence of the character, c
.
Example
#include <string.h>
#include <stdio.h>
int main(void)
{
char buf1[50] = "What time is it?";
char ch1 = 'm', ch2 = 'y';
char *ptr;
int res;
printf("buf1 : %s\n\n", buf1);
ptr = strrchr(buf1, ch1);
if (ptr != NULL)
{
res = ptr - buf1 + 1;
printf("%c found at position %d\n", ch1, res);
}
else
printf("%c not found\n", ch1);
printf("\n");
ptr = strrchr(buf1, ch2);
if (ptr != NULL)
{
res = ptr - buf1 + 1;
printf("%c found at position %d\n", ch2, res);
}
else
printf("%c not found\n", ch2);
}
Example Output
buf1 : What time is it?
m found at position 8
y not found