The-maddrqual=action
option indicates the
compiler’s response to non-standard memory qualifiers in C source code, as shown in the
table below.
Action | Response |
---|---|
require |
The qualifiers will be honored. If they cannot be met, an error will be issued. |
request |
The qualifiers will be honored, if possible. No error will be generated if they cannot be followed. |
ignore |
The qualifiers will be ignored and code compiled as if they were not used. |
reject |
If the qualifiers are encountered, an error will be immediately generated. |
The __near
qualifier is affected by this option. On PIC18
devices, this option affects the __far
qualifier; and for other 8-bit
devices, the __bank(x)
qualifier. By default, these qualifiers are
ignored; i.e., they are accepted without error, but have no effect. Using this option
allows these qualifiers to be interpreted differently by the compiler.
For example, when using the option -maddrqual=request
,
the compiler will try to honor any non-standard qualifiers, but silently ignore them if
they cannot be met.