A function that writes data to the EEPROM memory space.
Include
<xc.h>
Prototype
void eeprom_write(unsigned char address, unsigned char
value);
Arguments
address
value
Remarks
This function is available for all Mid-range devices that implement EEPROM. For PIC18 devices, calls to this routine will instead attempt to call the equivalent functions in the legacy PIC18 peripheral library, which you must download and install separately. It is recommended that for PIC18 devices you use MPLAB MCC to generate EEPROM access code, if possible.
This function tests and waits for any concurrent writes to EEPROM to conclude
before performing the required operation. The function will initiate the write of
value
to EEPROM at address
and this process will
still be taking place when the function returns. The new data written to EEPROM will
become valid at a later time. See your device data sheet for exact information about
EEPROM on your target device.
Example
#include <xc.h>
int main(void)
{
unsigned char data = 0x55;
unsigned char addr = 0x20;
eeprom_write(addr, data);
}