Calculates the trigonometric tangent function of a double precision floating-point value.
Include
<math.h>
Prototype
long double tanl(long double x);
Argument
x
Return Value
Returns the tangent of x
in radians.
Remarks
A domain error will occur if x
is a NaN or infinity.
Example
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
long double x, y;
errno = 0;
x = -1.0;
y = tanl(x);
if (errno)
perror("Error");
printf("The tangent of %Lf is %Lf\n", x, y);
errno = 0;
x = 0.0;
y = tanl(x);
if (errno)
perror("Error");
printf("The tangent of %Lf is %Lf\n", x, y);
}
Example Output
The tangent of -1.000000 is -1.557408
The tangent of 0.000000 is 0.000000