inline
specifier (see Inline Specifier) or #pragma
inline
. This is only a suggestion to the compiler and cannot always be obeyed.
Do not confuse this specifier/pragma with the intrinsic
pragma(1) (see The #pragma Intrinsic Directive), which
is for functions that have no corresponding source code and which will be specifically
expanded by the code generator during compilation.This specifier was originally named in-line
but was
changed to avoid confusion.