The USB driver can be installed even after Atmel Studio has been installed by following these steps:
Open "Control Panel" on the PC (Windows 95 and Windows NT does not support USB).
Select "Add or Remove Programs".
Select "Atmel Studio" or "Atmel Studio" in the list of programs.
Click on the "Change" button.
Select "Modify".
Select "Install/upgrade USB Driver".
The USB driver is now properly installed on the PC.
The Atmel AVR Dragon requires a USB port that can deliver 500mA (self-powered USB hub).