1.Create a new project in MPLAB® X IDE (for
ex: ATmega4808)
2.Open MCC by clicking Tools→ Embedded→ MPLAB® Code Configurator or click on
the MCC icon
3.Navigate to Versions[MCC] → MPLAB® Code
Configurator (Plugin) → Libraries → Microchip Technology, Inc. → AVR-IoT AWS Sensor Node.
Check the version of AVR IoT Sensor Node to ensure selection of library version 1.0.1. If
any other version is selected, double click on Library version 1.0.1.
4.In the Device Resources panel
navigate to Internet of Things → Examples → AVR-IoT AWS Sensor Node
5.Double click on AVR-IoT Sensor Node to
add this to the Project Resources panel
6.In the Project Resources panel
navigate to Internet of Things → Examples → AVR-IoT AWS Sensor Node
7.Ensure AVR-IoT AWS Sensor Node is
selected
8.AWS IoT Core
The firmware uses host endpoint as an entry point for an AWS web
service.
Default Endpoint: The AVR IoT AWS
Sensor Node uses the endpoint of Microchip's AWS account by default. This default
endpoint is stored in WINC15XX memory. Use the IoT Provisioning Tool to
permanently modify the default endpoint URL.
Custom Endpoint: Checking the 'Cloud
Configuration → Use custom endpoint URL' option in the GUI will allow the application
to use a custom endpoint. Enter the custom values for modifying the endpoint URL in
the respective sections. However, this will change the AWS endpoint URL only at
run-time. Use the IoT Provisioning Tool to permanently change
the default endpoint URL in the WINC15XX memory.
9.Click on the tooltip for more
information on each UI option.
10.Click Generate button
11.Connect the AVR-IoT WA Development Board
to the computer using a standard micro-USB cable
12.Build the firmware and program the hardware.
13.Additional information is available in
AVR IoT WA User Guide (Documentation
and Software → Documents).