To install the MPLAB® Code Configurator Plugin:
- 1.In MPLAB X IDE, select Plugins
from the Tools menu.
- 2.Select the Available Plugins
tab.
- 3.Check the box for the MPLAB® Code Configurator v5, and click on Install.
To install the library using Content Manager Tool (CMT):
- 1.Open MPLAB® Code Configurator
v5 from the Tools/Embedded menu.
- 2.Choose content type as Select MCC
Classic from Content Manager tab.
- 3.Under the "Optional" section, tick
the box beside AVR IoT AWS Sensor Node.
- 4.Click Finish from MCC
Content Manager Wizard.
To switch the library version in an existing project:
- 1.Open MPLAB® Code the
Tools/Embedded menu.
- 2.Click on Content Manager next
to Device Resources panel.
- 3.Expand Libraries component,
look up AVR IoT AWS Sensor Node and choose required version.
- 4.Click Apply.
To install the AVR IoT AWS Sensor Node Library offline:
- 1.Open the MPLAB Code Configurator
page: https://www.microchip.com/mcc .
- 2.Select the MPLAB Code Configurator
Downloads tab
- 3.Download AVR IoT AWS Sensor Node
(
avrIoTAWSSensorNode-1.0.2.mc3lib
).
- 4.In the MPLAB® X IDE, select
Options from the Tools menu
- 5.Select MPLAB® Code Configurator
v5.x tabfrom Plugins option
- 6.Click on Install Library
- 7.Browse to the location where you
saved the
avrIoTAWSSensorNode-1.0.2.mc3lib
, select and click
Open
- 8.Restart MPLAB® X IDE